# Intermittent image flickering / mixed frames when viewing ZED ROS 2 image topics on ROS 2 Jazzy

**URL:** <https://community.stereolabs.com/t/intermittent-image-flickering-mixed-frames-when-viewing-zed-ros-2-image-topics-on-ros-2-jazzy/11397>\
**Category:** ROS2\
**Tags:** ros2\
**Created:** [June 3, 2026, 11:52am UTC](https://community.stereolabs.com/t/intermittent-image-flickering-mixed-frames-when-viewing-zed-ros-2-image-topics-on-ros-2-jazzy/11397 "2026-06-03T11:52:30Z")\
**Posts on this page:** 4\
**Page:** 1

<div class="post-metadata">

**Author:** ![Sohaib-Snouber](https://community.stereolabs.com/user_avatar/community.stereolabs.com/sohaib-snouber/32/6281_2.png) [@Sohaib-Snouber](https://community.stereolabs.com/u/Sohaib-Snouber)\
**Post date:** [June 3, 2026, 11:52am UTC](https://community.stereolabs.com/t/intermittent-image-flickering-mixed-frames-when-viewing-zed-ros-2-image-topics-on-ros-2-jazzy/11397/1 "2026-06-03T11:52:30Z")

</div>

Hello,

I am using a ZED 2 camera with the ZED ROS 2 wrapper on ROS 2 Jazzy.

## Description

When viewing the camera directly in ZED Explorer, the image stream appears stable and correct. I monitored it for several minutes and did not observe any flickering or visual corruption.

However, when using the ROS 2 image topics published by the ZED ROS 2 wrapper, I occasionally observe image artifacts.

The artifacts appear as:

- Image flickering
- Partial mixing of two consecutive frames
- Regions of the image appearing to belong to different frames

The issue is intermittent and does not occur continuously.

## Additional testing

I initially observed the issue using:

```bash
rqt

```

subscribed to:

```plaintext
/zed/zed_node/rgb/color/rect/image

```

To rule out an RQt-specific issue, I also tested using:

```bash
ros2 run image_tools showimage --ros-args -r image:=/zed/zed_node/rgb/color/rect/image

```

and observed similar flickering/artifacts there as well.

Therefore, the issue does not appear to be limited to RQt Image View.

## Environment

- Camera: ZED 2
- OS: Ubuntu 24.04.4 LTS
- ROS 2: Jazzy
- Kernel: 6.17.0-29-generic
- CPU: AMD Ryzen 9 3900X
- GPU: NVIDIA RTX 4090
- NVIDIA Driver: 595.71.05
- CUDA: 13.2
- ZED SDK: 5.1.0
- ZED ROS 2 Wrapper commit:  
4719db300730c609efb6f6661a5d3d3fccb58bb7

## Diagnostics

- Camera detected correctly
- USB 3.0
- USB bandwidth reported as OK

The ZED Diagnostic tool reports multiple CUDA installations:

- CUDA 13.2
- CUDA 12.6

and recommends keeping only CUDA 13.

## Rosbag

I recorded a rosbag while reproducing the issue:

> **[zed\_flicker\_rosbag.tar.gz](https://cloud.hawk.de/index.php/s/KAdWbzXWxpN2sio)**
>
> HAWK Cloud - Hildesheim/Holzminden/Göttingen - Wir sind HAWK.

Bag details:

- Topic: `/zed/zed_node/rgb/color/rect/image`
- Duration: ~3 seconds
- Messages: 85
- Approximate frame rate: ~29 FPS

## Question

Since the image stream is stable in ZED Explorer but shows artifacts when viewed through ROS 2 topics, what additional diagnostics would you recommend to determine whether the issue originates from:

- The ROS 2 wrapper
- ROS 2 image transport
- DDS/QoS configuration
- GPU/OpenGL rendering
- Another component in the ROS visualization pipeline

Thank you.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [June 3, 2026, 3:27pm UTC](https://community.stereolabs.com/t/intermittent-image-flickering-mixed-frames-when-viewing-zed-ros-2-image-topics-on-ros-2-jazzy/11397/2 "2026-06-03T15:27:09Z")

</div>

Hi @Sohaib-Snouber  
Welcome to the [StereoLabs](https://www.stereolabs.com/) community.

> [@Sohaib-Snouber](#):
>
> However, when using the ROS 2 image topics published by the ZED ROS 2 wrapper, I occasionally observe image artifacts.

This could happen due to an overload of the system, causing buffer overflows in the USB3 controller.

> [@Sohaib-Snouber](#):
>
> The artifacts appear as:
> 
> - Image flickering
> - Partial mixing of two consecutive frames
> - Regions of the image appearing to belong to different frames
> 
> The issue is intermittent and does not occur continuously.

This confirms the previous hypothesis.

I recommend you:

- use the latest version of the ZED SDK. The version v5.1.1 is pretty old.
- use the latest version of the ZED ROS2 Wrapper
- read this section of the documentation to learn how to set up the ROS 2 environment to obtain the best performance: [DDS Middleware and Network tuning - Stereolabs](https://www.stereolabs.com/docs/ros2/dds-and-network-tuning)
- read this section of the documentation to learn how to optimize the the ZED nodes: [Node Frequency Tuning - Stereolabs](https://www.stereolabs.com/docs/ros2/frequency-tuning)

---

<div class="post-metadata">

**Author:** ![Sohaib-Snouber](https://community.stereolabs.com/user_avatar/community.stereolabs.com/sohaib-snouber/32/6281_2.png) [@Sohaib-Snouber](https://community.stereolabs.com/u/Sohaib-Snouber)\
**Post date:** [October 6, 2026, 12:39pm UTC](https://community.stereolabs.com/t/intermittent-image-flickering-mixed-frames-when-viewing-zed-ros-2-image-topics-on-ros-2-jazzy/11397/3 "2026-10-06T12:39:34Z")

</div>

Hi, I investigated this further and I can now reproduce the corrupted/mixed frame below ROS 2.

I updated to ZED SDK 5.5.0 and zed-ros2-wrapper v5.5.0, and the issue still occurs.

I then captured the ZED stream directly through Linux V4L2 using MMAP at 3840x1080 YUYV @ 30 FPS, without ROS 2, DDS, rqt, or the ZED ROS wrapper.

I captured a bad buffer with an expected frame size of 8294400 bytes, but bytesused was only 3668672 bytes. The buffer also had flags 0x12041. The bad frame had sequence 1097, and the next normal frame had sequence 1099 with the full 8294400 bytes.

Visually, this produces the same mixed/shifted frame sections I reported before.

So the corruption is already present at the V4L2 level as an incomplete/error frame, which strongly suggests that ROS 2 is not the root cause.

There is also a very similar report here: [https://github.com/stereolabs/zed-ros2-wrapper/issues/287](https://github.com/stereolabs/zed-ros2-wrapper/issues/287)

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [October 7, 2026, 11:34am UTC](https://community.stereolabs.com/t/intermittent-image-flickering-mixed-frames-when-viewing-zed-ros-2-image-topics-on-ros-2-jazzy/11397/4 "2026-10-07T11:34:13Z")

</div>

Hi @Sohaib-Snouber,  
thank you for the detailed investigation, this is very useful information.

> [@Sohaib-Snouber](#):
>
> I captured a bad buffer with an expected frame size of 8294400 bytes, but bytesused was only 3668672 bytes. The buffer also had flags 0x12041. The bad frame had sequence 1097, and the next normal frame had sequence 1099 with the full 8294400 bytes.

This confirms the hypothesis of my previous reply. The flags value `0x12041` includes `V4L2_BUF_FLAG_ERROR` (`0x40`), which the `uvcvideo` kernel driver sets when it does not receive the full payload of a frame from the USB link. The sequence jump from 1097 to 1099 also shows that a frame was lost. The data is lost between the camera and the host USB3 controller, before the ZED SDK, the ZED ROS 2 Wrapper, or ROS 2 can access it.

> [@Sohaib-Snouber](#):
>
> So the corruption is already present at the V4L2 level as an incomplete/error frame, which strongly suggests that ROS 2 is not the root cause.

Correct, the root cause is the USB3 connection. The most common causes are:

- USB3 ports on the front panel or on case extensions, which are connected to the motherboard by internal wires; use a port on the rear I/O panel soldered directly to the motherboard
- USB3 hubs, cable extenders, or non-original cables; use the original [StereoLabs](https://www.stereolabs.com/) USB3 cable and check that the connector screws are fully tightened
- The USB3 controller shared with other high-bandwidth devices
- An outdated BIOS; some AMD Ryzen platforms had known USB data loss issues that were fixed by BIOS (AGESA) updates
- USB autosuspend; you can disable it by adding `usbcore.autosuspend=-1` to the kernel boot parameters

You can check `sudo dmesg -w | grep -i -E "xhci|uvc|usb"` while the issue occurs to see if the kernel reports errors on the USB bus.

If no free port on the motherboard solves the problem, a dedicated PCIe USB3 expansion card normally provides a reliable connection.

Finally, keep `general.enable_image_validity_check` set to `1` in the [common\_stereo.yaml](https://github.com/stereolabs/zed-ros2-wrapper/blob/master/zed_wrapper/config/common_stereo.yaml) file, so the ZED SDK checks each frame for corruption before processing it.