# Intermittent detection issue – only 3 out of 4 ZED X cameras detected on ZED Box Orin NX (driver 1.3.2, JetPack 6.0)

**URL:** <https://community.stereolabs.com/t/intermittent-detection-issue-only-3-out-of-4-zed-x-cameras-detected-on-zed-box-orin-nx-driver-1-3-2-jetpack-6-0/10484>\
**Category:** ZED X\
**Created:** [December 5, 2025, 6:59am UTC](https://community.stereolabs.com/t/intermittent-detection-issue-only-3-out-of-4-zed-x-cameras-detected-on-zed-box-orin-nx-driver-1-3-2-jetpack-6-0/10484 "2025-12-05T06:59:41Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![tiedvards](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/t/dc4da7/32.png) [@tiedvards](https://community.stereolabs.com/u/tiedvards)\
**Post date:** [December 5, 2025, 6:59am UTC](https://community.stereolabs.com/t/intermittent-detection-issue-only-3-out-of-4-zed-x-cameras-detected-on-zed-box-orin-nx-driver-1-3-2-jetpack-6-0/10484/1 "2025-12-05T06:59:41Z")

</div>

Hello [Stereolabs](https://www.stereolabs.com/) Support,

I’m experiencing an intermittent issue with a 4-camera GMSL setup where only three out of four ZED X cameras are detected on startup.

**System details:**

- Hardware: ZED Box Orin NX 16 GB

- Cameras: 4× ZED X

- OS: Jetson Linux R36.3.0 / JetPack 6.0

- Driver: `was 1.3.1 (decided update to 1.3.2, but doesnt help)`

- [Stereolabs](https://www.stereolabs.com/) ZED SDK Version : 5.0.7

**Issue:**

- After a cold boot or reboot, `ZED_Explorer -a` usually reports only **3 cameras** instead of 4.

- The 4th camera behaves as if it is not connected: it does not appear in `ZED_Explorer -a`, and my application also only sees 3 cameras.

- Sometimes this 4th camera is recognized later, without any physical changes to the wiring, so the problem is intermittent.

- When the issue occurs, there are no obvious error messages related to that camera in `dmesg` (at least nothing clearly indicating a failed GMSL link for that port).

**Questions:**

1. Are there any recommended debug steps or tools to check the GMSL link status per port (specific kernel logs, devicetree checks, additional configuration) to determine whether this is a hardware or driver issue?

2. Would it be helpful if I provide logs such as `dmesg`, the output of `ZED_Explorer -a`, and `ZED_Diagnostic -c` for the cases when only 3 cameras are detected?

Best regards,

Ti Ed

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [December 9, 2025, 4:53pm UTC](https://community.stereolabs.com/t/intermittent-detection-issue-only-3-out-of-4-zed-x-cameras-detected-on-zed-box-orin-nx-driver-1-3-2-jetpack-6-0/10484/2 "2025-12-09T16:53:00Z")

</div>

Hi @tiedvards  
please upgrade the ZED SDK to v5.1.1 and try to use the ZED\_Studio tool to open the 4 cameras simultaneously.

Please remember that the maximum FPS when using 4 cameras is halfed:

> **[ZED Box Orin - Stereolabs](https://www.stereolabs.com/docs/embedded/zed-box-orin#gmsl2-option)**
>
> Congratulations on being the owner of a brand-new ZED Box embedded PC!