# I'm not be able to openning and clossing secuently the camera using threads from pyqt6

**URL:** <https://community.stereolabs.com/t/im-not-be-able-to-openning-and-clossing-secuently-the-camera-using-threads-from-pyqt6/9012>\
**Category:** Python\
**Tags:** linux, python, sdk, jetson\
**Created:** [June 6, 2025, 3:29pm UTC](https://community.stereolabs.com/t/im-not-be-able-to-openning-and-clossing-secuently-the-camera-using-threads-from-pyqt6/9012 "2025-06-06T15:29:52Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![claudiomla](https://community.stereolabs.com/user_avatar/community.stereolabs.com/claudiomla/32/4491_2.png) [@claudiomla](https://community.stereolabs.com/u/claudiomla)\
**Post date:** [June 6, 2025, 3:29pm UTC](https://community.stereolabs.com/t/im-not-be-able-to-openning-and-clossing-secuently-the-camera-using-threads-from-pyqt6/9012/1 "2025-06-06T15:29:52Z")

</div>

After successfully opening and closing a ZED-X camera with the ZED SDK in Python (using a QThread from qt6), all subsequent attempts to open the camera (in new threads) fail. The SDK returns a camera open error, and dmesg shows ‘probe failed with error -1’ and ‘serializer initialization failed’ for the ZED-X sensor (MAX96712).

For each thread, I open the camera, take a picture and close the camera, but when I repeat the program break.

Even after deleting the camera object, doing explicit garbage collection, and waiting several seconds (busy-wait), the device cannot be re-initialized without rebooting the system.

But if I do it in the **main thread** (sequentially in a loop, using a for), the camera opens and closes successfully every time.

This test was created by ChatGPT but works to proof my point.

```auto
import sys
import time
import traceback
import pyzed.sl as sl
import gc

from PyQt6.QtCore import QThread, pyqtSignal, QObject, QCoreApplication

# --- CONFIG BLOCK ---
CONFIG = {
    "max_cycles": 10, # How many times to open/close
    "sleep_between": 2, # Seconds between close and next open
    "resolution": sl.RESOLUTION.HD1080,
    "fps": 15,
    "depth_mode": sl.DEPTH_MODE.NEURAL,
    "timeout_on_open": 8, # Not used - for future
    "verbose": True
}

class CameraThread(QThread):
    finished_signal = pyqtSignal(int, str) # ciclo, resultado

    def __init__ (self, cfg, cycle_id):
        super(). __init__ ()
        self.cfg = cfg
        self.cycle_id = cycle_id

    def run(self):
        reslog = ""
        cam = None
        try:
            # --- OPEN ---
            if self.cfg["verbose"]:
                print(f"[Ciclo {self.cycle_id}] Opening ZED camera (QThread)...")
            cam = sl.Camera()
            init_params = sl.InitParameters(
                camera_resolution=self.cfg["resolution"],
                camera_fps=self.cfg["fps"],
                depth_mode=self.cfg["depth_mode"],
                coordinate_units=sl.UNIT.METER,
                coordinate_system=sl.COORDINATE_SYSTEM.RIGHT_HANDED_Y_UP,
                sdk_verbose=0
            )
            err = cam.open(init_params)
            cam.enable_positional_tracking()
            if err != sl.ERROR_CODE.SUCCESS:
                print(f"[Ciclo {self.cycle_id}] ❌ Open error: {err}")
                reslog = f"OPEN FAILED ({err})"
                return
            print(f"[Ciclo {self.cycle_id}] ✅ Camera opened!")

            # --- GRAB ---
            mat = sl.Mat()
            status = cam.grab()
            if status == sl.ERROR_CODE.SUCCESS:
                cam.retrieve_image(mat, sl.VIEW.LEFT)
                print(f"[Ciclo {self.cycle_id}] Image grab OK")
                reslog = "SUCCESS"
            else:
                print(f"[Ciclo {self.cycle_id}] Grab failed: {status}")
                reslog = f"GRAB FAILED ({status})"

            # --- CLOSE ---
            try:
                cam.disable_positional_tracking()
            except Exception:
                print(f"[Ciclo {self.cycle_id}] disable_positional_tracking() failed (maybe not enabled)")
            try:
                cam.close()
                print(f"[Ciclo {self.cycle_id}] Camera closed.")
            except Exception as e:
                print(f"[Ciclo {self.cycle_id}] Camera close error: {e}")

            del cam
            cam = None
            gc.collect()
            print(f"[Ciclo {self.cycle_id}] GC done.")

        except Exception as e:
            print(f"[Ciclo {self.cycle_id}] EXCEPTION: {e}")
            print(traceback.format_exc())
            reslog = f"EXCEPTION {e}"
        finally:
            # Emite señal de terminado para el ciclo
            self.finished_signal.emit(self.cycle_id, reslog)

def run_camera_cycles_qt(config):
    from PyQt6.QtWidgets import QApplication
    app = QApplication(sys.argv)
    logs = []

    def on_cycle_finished(cycle_id, result):
        print(f"=== Ciclo {cycle_id} terminado: {result} ===")
        logs.append(f"Cycle {cycle_id}: {result}")
        # Lanza el próximo ciclo o sale si ya son todos
        run_next_cycle(cycle_id + 1)

    def run_next_cycle(cycle):
        if cycle > config["max_cycles"]:
            print("==== TODOS LOS CICLOS HECHOS ====")
            for log in logs:
                print(log)
            QCoreApplication.quit()
            return

        print(f"\n--- Lanzando ciclo {cycle} ---")
        thread = CameraThread(config, cycle)
        # Necesario: guardar referencia hasta terminar, sino el thread es recolectado antes de tiempo
        threads.append(thread)
        thread.finished_signal.connect(on_cycle_finished)
        thread.start()

    threads = []
    run_next_cycle(1)
    app.exec()

if __name__ == " __main__":
    run_camera_cycles_qt(CONFIG)

```

---

<div class="post-metadata">

**Author:** ![hbeaumont](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/h/67e7ee/32.png) [@hbeaumont](https://community.stereolabs.com/u/hbeaumont)\
**Post date:** [June 10, 2025, 1:51pm UTC](https://community.stereolabs.com/t/im-not-be-able-to-openning-and-clossing-secuently-the-camera-using-threads-from-pyqt6/9012/2 "2025-06-10T13:51:21Z")

</div>

Hello Claudiomla,

Welcome on our forum and thank you for your message.  
I ran your script and it worked. I used the latest verison of SDK that you can find here: [ZED SDK 5.0 - Download | Stereolabs](https://www.stereolabs.com/en-fr/developers/release/5.0#82af3640d775)  
Please ugrade it if it is not done yet.

I hope this will resolve your issue, but do not hesitate to reach us again if you still have issues.

Best regards,