# How to improve point cloud frame rate on Orin NX (16GB) + ZED X via GMSL2 Capture Card Mono

**URL:** <https://community.stereolabs.com/t/how-to-improve-point-cloud-frame-rate-on-orin-nx-16gb-zed-x-via-gmsl2-capture-card-mono/9408>\
**Category:** ZED X\
**Tags:** ros, jetson, depth\
**Created:** [July 15, 2025, 11:35am UTC](https://community.stereolabs.com/t/how-to-improve-point-cloud-frame-rate-on-orin-nx-16gb-zed-x-via-gmsl2-capture-card-mono/9408 "2025-07-15T11:35:47Z")\
**Posts on this page:** 3\
**Page:** 1

<div class="post-metadata">

**Author:** ![Lincoln\_Liu](https://community.stereolabs.com/user_avatar/community.stereolabs.com/lincoln_liu/32/4662_2.png) [@Lincoln\_Liu](https://community.stereolabs.com/u/Lincoln_Liu)\
**Post date:** [July 15, 2025, 11:35am UTC](https://community.stereolabs.com/t/how-to-improve-point-cloud-frame-rate-on-orin-nx-16gb-zed-x-via-gmsl2-capture-card-mono/9408/1 "2025-07-15T11:35:47Z")

</div>

Hi all,  
I’m currently using the ZED X camera with a GMSL2 Capture Card Mono connected to an NVIDIA Jetson Orin NX (16GB), running on the official NVIDIA Orin Nano Dev Kit carrier board.  
I’m using ROS and the [Stereolabs](https://www.stereolabs.com/) ZED ROS1 wrapper, and have already tried modifying parameters in both `zedx.yaml` and `common.yaml` (including `grab_frame_rate`, `depth_mode`, and resolution). However, no matter how I tune the settings, the effective point cloud frame rate always stays at around 12 Hz (even though the target is 30 Hz).  
I’ve also verified that `/zedx/zed_node/point_cloud/cloud_registered` is being published at this limited rate, and system resources (CPU/GPU) on the Orin NX seem underutilized. And I’ve tested both `ULTRA` and `PERFORMANCE` depth modes.  
My questions are:

1. What parameters or settings should I configure to reach 30 Hz point cloud update rate on this setup?
2. Does the GMSL2 Capture Card Mono or carrier board impose any limitations on data throughput or frame rate?
3. Are there known limitations on ZED SDK or ROS wrapper for ZED X under Orin NX that cap performance?  
Any tips or working configurations from others using similar setups would be greatly appreciated!

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [July 16, 2025, 10:20am UTC](https://community.stereolabs.com/t/how-to-improve-point-cloud-frame-rate-on-orin-nx-16gb-zed-x-via-gmsl2-capture-card-mono/9408/2 "2025-07-16T10:20:00Z")

</div>

Hi @Lincoln_Liu  
Welcome to the [StereoLabs](https://www.stereolabs.com/) community.

I recommend you switch to ROS 2 to use the improved features that we introduced with the [ZED ROS2 Wrapper](https://www.stereolabs.com/docs/ros2).

ROS 1 is EOL and we are not improving the relative Wrapper anymore.

---

<div class="post-metadata">

**Author:** ![Lincoln\_Liu](https://community.stereolabs.com/user_avatar/community.stereolabs.com/lincoln_liu/32/4662_2.png) [@Lincoln\_Liu](https://community.stereolabs.com/u/Lincoln_Liu)\
**Post date:** [July 16, 2025, 11:21am UTC](https://community.stereolabs.com/t/how-to-improve-point-cloud-frame-rate-on-orin-nx-16gb-zed-x-via-gmsl2-capture-card-mono/9408/3 "2025-07-16T11:21:34Z")

</div>

OK thanks, I’ll try it