# High CPU Usage When Running Dual ZED2i Cameras via ROS1 – Optimization Suggestions?

**URL:** <https://community.stereolabs.com/t/high-cpu-usage-when-running-dual-zed2i-cameras-via-ros1-optimization-suggestions/8888>\
**Category:** ROS1\
**Tags:** multi-camera, sdk\
**Created:** [May 23, 2025, 9:21am UTC](https://community.stereolabs.com/t/high-cpu-usage-when-running-dual-zed2i-cameras-via-ros1-optimization-suggestions/8888 "2025-05-23T09:21:05Z")\
**Posts on this page:** 4\
**Page:** 1

<div class="post-metadata">

**Author:** ![MarkdDk](https://community.stereolabs.com/user_avatar/community.stereolabs.com/markddk/32/4431_2.png) [@MarkdDk](https://community.stereolabs.com/u/MarkdDk)\
**Post date:** [May 23, 2025, 9:21am UTC](https://community.stereolabs.com/t/high-cpu-usage-when-running-dual-zed2i-cameras-via-ros1-optimization-suggestions/8888/1 "2025-05-23T09:21:05Z")

</div>

Hi everyone,

We are currently operating **two ZED2i cameras** in a ROS1 (Noetic) environment using the following setup, and we’ve noticed **unexpectedly high CPU utilization (around 20~25%)** even with relatively default settings. I’m hoping to get some insights into potential optimizations.

* * *

### 🔧 **System Configuration**

**Hardware** :

- 2x ZED2i cameras (connected via 10m USB repeater cables)
- Intel Core i7-12700 (12-core, 2.1GHz, 25MB cache)
- NVIDIA RTX 4060 8GB
- 2x DDR5 4800MHz SODIMM
- USB 3.0 direct connection to the industrial PC motherboard

**Software** :

- Ubuntu 20.04
- ROS1 Noetic
- ZED SDK 4.1.3
- CUDA 12.5 / Driver 555.42.02
- Camera settings: **HD2K resolution** with **Neural Depth** enabled

* * *

### 📦 **ROS Integration Method**

We’re launching each camera using this custom wrapper pattern:

```auto
<!--zed_connector_for_multi-->
<launch>
    <arg name="publish_urdf" default="false" />

    <!-- CAMERA connect info. -->
    <arg name="node_name" default="ZED" />
    <arg name="serial_number" default="12345678" /> 
    <arg name="camera_model" default="zed2i" />
    <arg name="camera_name" default="up0" />

    <group ns="$(arg camera_name)">
        <include file="$(find zed_wrapper)/launch/include/zed_camera_mod.launch">
            <arg name="serial_number" value="$(arg serial_number)" />
            <arg name="camera_name" value="$(arg camera_name)" />
            <arg name="node_name" value="$(arg node_name)" />
            <arg name="camera_model" value="$(arg camera_model)" />
            <arg name="publish_urdf" value="$(arg publish_urdf)" />
            <arg name="publish_tf" value="false" />
            <arg name="camera_id" value="0" />
        </include>
    </group>
</launch>
----------------------------------------------------------------------------------------------------------------------------------------------------
<include file="$(find zed_wrapper)/launch/zed_connector_for_multi.launch">
  <arg name="camera_name" value="$(arg loc1)"/>
  <arg name="serial_number" value="$(arg serial_number1)"/>
</include>
<include file="$(find zed_wrapper)/launch/zed_connector_for_multi.launch">
  <arg name="camera_name" value="$(arg loc2)"/>
  <arg name="serial_number" value="$(arg serial_number2)"/>
</include>

```

Each `zed_connector_for_multi.launch` instance passes args into `zed_camera_mod.launch` with default settings except `publish_tf:=false`.

We then subscribe to both `rgb` and `pointcloud` topics, and forward the data through a custom service every **3.3 seconds**.

* * *

### ❗ **The Problem**

Despite using relatively low-frequency ROS usage (every 3.3s), we are observing:

- ~ **20–25% CPU utilization** consistently across the 12-core CPU
- This is **without any subscribers** doing heavy work or visualization (just background publishing)

* * *

### 🙋‍♂️ **Question**

- Is this level of CPU usage expected under the above setup?
- Are there any **ZED SDK or ROS launch settings** that could reduce CPU load, especially when running two cameras?
- Would using `performance_mode`, reducing frame rate/resolution, or launching in a certain sequence help?
- Would offloading more work to the GPU be possible?

Any suggestions on how to **optimize CPU load in a dual ZED2i + ROS1 system** would be greatly appreciated!

Thanks in advance for your support. 🙏

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [May 23, 2025, 9:41am UTC](https://community.stereolabs.com/t/high-cpu-usage-when-running-dual-zed2i-cameras-via-ros1-optimization-suggestions/8888/2 "2025-05-23T09:41:01Z")

</div>

Hi @MarkdDk  
Welcome to the [StereoLabs](https://www.stereolabs.com/) community.

First of all, I would like to recommend upgrading to ROS 2 for two reasons:

1. ROS Noetic is going EOL in 8 days
2. The ZED ROS Wrapper is no more maintained and we are not upgrading it with the latest new ZED SDK features

> [@MarkdDk](#):
>
> Is this level of CPU usage expected under the above setup?

Even if you are not subscribing to topics, if the depth mode is different from `NONE` the ZED SDK performs depth processing at the grab rate to retrieve camera position information. So this CPU load is expected when using two cameras

> [@MarkdDk](#):
>
> Are there any **ZED SDK or ROS launch settings** that could reduce CPU load, especially when running two cameras?

What features do you need?

> [@MarkdDk](#):
>
> Would using `performance_mode`, reducing frame rate/resolution, or launching in a certain sequence help?

What are you referring to?

> [@MarkdDk](#):
>
> Would offloading more work to the GPU be possible?

What do you mean?

---

<div class="post-metadata">

**Author:** ![MarkdDk](https://community.stereolabs.com/user_avatar/community.stereolabs.com/markddk/32/4431_2.png) [@MarkdDk](https://community.stereolabs.com/u/MarkdDk)\
**Post date:** [May 23, 2025, 10:09am UTC](https://community.stereolabs.com/t/high-cpu-usage-when-running-dual-zed2i-cameras-via-ros1-optimization-suggestions/8888/3 "2025-05-23T10:09:29Z")

</div>

Thank you for your response.  
I have a few follow-up questions:

1. I noticed that the frame rate always seems to be fixed at 15 FPS.  
Is there a way to reduce it to 5 Hz operation?
2. Is it possible to retrieve image and depth data using a **trigger-based** method instead of continuous **streaming mode**?

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [May 23, 2025, 10:35am UTC](https://community.stereolabs.com/t/high-cpu-usage-when-running-dual-zed2i-cameras-via-ros1-optimization-suggestions/8888/4 "2025-05-23T10:35:47Z")

</div>

> [@MarkdDk](#):
>
> I noticed that the frame rate always seems to be fixed at 15 FPS.  
> Is there a way to reduce it to 5 Hz operation?

This is not possible with the ZED ROS Wrapper. It’s possible with the ZED ROS2 Wrapper.

> [@MarkdDk](#):
>
> Is it possible to retrieve image and depth data using a **trigger-based** method instead of continuous **streaming mode**?

No, this feature is not provided by the camera.