# Grab() takes a fixed faster path on ~1/3 of frames on two units, persists across restart and Camera::reboot (SDK 5.2.3, NEURAL)

**URL:** <https://community.stereolabs.com/t/grab-takes-a-fixed-faster-path-on-1-3-of-frames-on-two-units-persists-across-restart-and-camera-reboot-sdk-5-2-3-neural/11848>\
**Category:** Software\
**Created:** [November 16, 2026, 8:36pm UTC](https://community.stereolabs.com/t/grab-takes-a-fixed-faster-path-on-1-3-of-frames-on-two-units-persists-across-restart-and-camera-reboot-sdk-5-2-3-neural/11848 "2026-11-16T20:36:32Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![jeff.crouse](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/j/e99b99/32.png) [@jeff.crouse](https://community.stereolabs.com/u/jeff.crouse)\
**Post date:** [November 16, 2026, 8:36pm UTC](https://community.stereolabs.com/t/grab-takes-a-fixed-faster-path-on-1-3-of-frames-on-two-units-persists-across-restart-and-camera-reboot-sdk-5-2-3-neural/11848/1 "2026-11-16T20:36:32Z")

</div>

Hi @Myzhar, Related background is in 11545, but this looks like a different behavior.

Two of our seven on-site boxes have switched into a state where about a third of `grab()` calls take a fixed, much shorter time than normal. The camera looks fine, depth looks fine by the one measure we have, and nothing we’ve tried clears it. So the real question is: what is `grab()` doing differently on those frames?

## Setup

- ZED Box Mini (Orin Nano 8GB, 15W mode), ZED 2i over USB, ZED SDK **5.2.3**
- `HD1080` @ 30 fps, `DEPTH_MODE::NEURAL`, positional tracking + object detection enabled
- One process per box, the same config on all seven

## What we measured

Five samples a minute apart, each over the last 60 frames:

| | 5 healthy boxes | 2 affected boxes |
| --- | --- | --- |
| Share of loop iterations that take the very next camera frame (33 ms image-timestamp gap) | 0.00 - 0.02 | **0.27 - 0.45** |
| `grab()` wall time, median | ~60 ms | 47 - 55 ms |
| `grab()` wall time, 10th percentile | 46 - 59 ms | **36.3 - 37.0 ms on BOTH boxes** |
| Loop rate | ~15 Hz | ~19.5 Hz |

On a healthy box every `grab()` takes ~60 ms and every iteration skips exactly one camera frame (67 ms gaps). On the two affected boxes there are two distinct `grab()` times, ~60 ms and a tight ~37 ms, and the ~37 ms value is the same on both units. That looks like a different code path, not noise.

## What we ruled out

- **The camera.** Image timestamps still advance by 33 ms steps, so it still delivers 30 fps. Exposure and gain read the same range as the healthy boxes (exposure 90 - 100 everywhere). Repeated frames are ~0, so these are new images.
- **Depth quality, roughly.** The valid-pixel ratio over the whole frame stays at each box’s normal value.
- **The host config.** Same power mode, GPU at max clock, same SDK version, and the optimized model files were built in September, before either box changed.
- **Time of day / lighting.** The rate is flat from 05:00 to 22:00.

## What clears it (nothing so far)

- Process restart: no (daily, and dozens of times since)
- `Camera::reboot(sn, true)`: no (tried once on one of the boxes)
- Full power cycle: not tried yet

## Timeline

- Box A switched on 2026-11-04, about an hour after a scheduled close + reopen of the camera at 05:30.
- Box B came up in this state straight from the same 05:30 reopen on 2026-11-11.
- No USB errors or re-enumerations at either onset. Both boxes did develop the worst USB link error counts in our fleet in the days AFTER, and both have since hit the zero-filled image fault from 11545 more than the others. That could be coincidence on two boxes, but I didn’t want to leave it out.

## Questions

1. Is there a path inside `grab()` that skips or reuses part of the NEURAL depth computation on some frames? ~37 ms vs ~60 ms is consistent with that, but I may be missing something.
2. If so, what puts the SDK into it, and why would it survive a process restart and a `Camera::reboot`? Is there any state the SDK persists on disk or in the driver that we should clear?
3. Is there a way to detect it from the API, or to force the normal path?
4. Is this known, and is it different on 5.4.x or 5.5?

Happy to send per-box logs, the depth/left/right captures, or run a test build on one of the affected boxes. We can also try a full power cycle if that would tell you something.