# GPU Usage/Power Issues Using ZED2 with Jetson Xavier NX

**URL:** <https://community.stereolabs.com/t/gpu-usage-power-issues-using-zed2-with-jetson-xavier-nx/9899>\
**Category:** ZED2\
**Tags:** zed-sdk, ros, sdk, jetson, depth\
**Created:** [September 16, 2025, 11:47am UTC](https://community.stereolabs.com/t/gpu-usage-power-issues-using-zed2-with-jetson-xavier-nx/9899 "2025-09-16T11:47:15Z")\
**Posts on this page:** 1\
**Showing post:** 7

<div class="post-metadata">

**Author:** ![selim](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/s/51bf81/32.png) [@selim](https://community.stereolabs.com/u/selim)\
**Post date:** [September 19, 2025, 7:37am UTC](https://community.stereolabs.com/t/gpu-usage-power-issues-using-zed2-with-jetson-xavier-nx/9899/7 "2025-09-19T07:37:52Z")

</div>

Hi @Myzhar ,

Thank you for your time trying to help me but I think I didn’t clarify enough my system.

When using ZED2’s NEURAL modes, GPU usage of my Jetson Xavier NX climbs to 99% and OC\_ALARM warnings are frequently logged on message buffer of the kernel. After couple of seconds, Jetson forces itself to shutdown. When I try to use the depreciated modes, they also give OC\_ALARM warning but not that frequently. So, I am able to work with them. My biggest question for the time being is that: Is it suitable to use ZED2 cam with Jetson Xavier NX? According to **[your answer](https://community.stereolabs.com/t/low-framerate-for-depth-image-on-jetson-xavier-nx/1841/4)**, it is possible and I should expect 18FPS using ULTRA mode. However, these depreciated modes’ depth calculation is not good enough and not even close to NEURAL mode calculations.

Also, it is clear that I am debugging the system using a remote machine not to load the Jetson with GUI stuff. Using the common network, I can see all the topics that are published on Jetson.

Up to now, I couldn’t improve my depth calculation quality but increased the fps modifying the publish rate parameters. However, I need quality over rate. So, I need to somehow use the NEURAL modes on my Jetson. If I cannot do that, I should either dedicate one Jetson only for running ZED2 or change my stereo depth cam.

Thanks,  
Selim

---

_[View the full topic](https://community.stereolabs.com/t/gpu-usage-power-issues-using-zed2-with-jetson-xavier-nx/9899)._