# GPIO Triggering on ZED Box 2 Max - T5000

**URL:** <https://community.stereolabs.com/t/gpio-triggering-on-zed-box-2-max-t5000/11825>\
**Category:** ZED Box\
**Created:** [October 29, 2026, 2:10pm UTC](https://community.stereolabs.com/t/gpio-triggering-on-zed-box-2-max-t5000/11825 "2026-10-29T14:10:56Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![poel\_da](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/b2d939/32.png) [@poel\_da](https://community.stereolabs.com/u/poel_da)\
**Post date:** [October 29, 2026, 2:10pm UTC](https://community.stereolabs.com/t/gpio-triggering-on-zed-box-2-max-t5000/11825/1 "2026-10-29T14:10:56Z")

</div>

We are thinking of getting a ZED Box 2 Max - T5000. Is the [GPIO Triggering](https://docs.stereolabs.com/docs/products/embedded/zed-link-capture-card/gmsl2/zed-link-quad/zed-link-quad-gpio-triggering) like for the ZED Link Capture Cards also available on this platform? We currently use trigger signals for our ZED X cameras and would like to continue with this workflow.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [October 29, 2026, 6:57pm UTC](https://community.stereolabs.com/t/gpio-triggering-on-zed-box-2-max-t5000/11825/2 "2026-10-29T18:57:51Z")

</div>

Hi @poel_da,  
Welcome to the [StereoLabs](http://www.stereolabs.com) community.

> [@poel\_da](#):
>
> Is the [GPIO Triggering](https://docs.stereolabs.com/docs/products/embedded/zed-link-capture-card/gmsl2/zed-link-quad/zed-link-quad-gpio-triggering) like for the ZED Link Capture Cards also available on this platform?

No, the [ZED Box 2 Max - T5000](https://www.stereolabs.com/store/products/zed-box-2-max-t5000) does not expose the camera trigger signals on an external connector. The eight GMSL2 cameras are hardware-synchronized by the deserializers. To align them with other devices, synchronize the system clocks, for example with PTP over Ethernet. See the [Camera synchronization](https://docs.stereolabs.com/docs/products/embedded/zed-box-series/zed-box-2-max/using-gmsl#camera-synchronization) section of the documentation.

> [@poel\_da](#):
>
> We currently use trigger signals for our ZED X cameras and would like to continue with this workflow

If you need external trigger signals, the [ZED Box 2](https://www.stereolabs.com/store/products/zed-box-2) is the right choice. Its Sync and IO connector supports both trigger output (`sync_mode=1`) and external trigger input (`sync_mode=2`), as described in the [ZED Box 2 Camera synchronization](https://docs.stereolabs.com/docs/products/embedded/zed-box-series/zed-box-2/using-gmsl#camera-synchronization) guide. Note that its trigger pins are 1.8V signals, so a level shifter is required if your current trigger source is 3.3V or 5V.