# Frequency differences between recieved and published images 

**URL:** <https://community.stereolabs.com/t/frequency-differences-between-recieved-and-published-images/11465>\
**Category:** ROS2\
**Created:** [June 22, 2026, 12:38pm UTC](https://community.stereolabs.com/t/frequency-differences-between-recieved-and-published-images/11465 "2026-06-22T12:38:30Z")\
**Posts on this page:** 3\
**Page:** 1

<div class="post-metadata">

**Author:** ![Piotr.Klimaszew](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/a183cd/32.png) [@Piotr.Klimaszew](https://community.stereolabs.com/u/Piotr.Klimaszew)\
**Post date:** [June 22, 2026, 12:38pm UTC](https://community.stereolabs.com/t/frequency-differences-between-recieved-and-published-images/11465/1 "2026-06-22T12:38:30Z")

</div>

Hallo,

I have problem because there is a big difference between recieved and published frequency. I have setup which consist of Jetson Orin and laptop through ethernet cable. Both have the same version of ROS2 installed → Humble.

I publish video captured by camera using default zdk publisher from ZED SDK using ROS2( $ ros2 launch zed\_wrapper zed\_camera.launch.py camera\_model:=zedx). I turned off depth perception and similar modules. Following gDDS and Network Tuning I changed the parameters to the value suggest in it. I have increased the compression to the 4.0. The publisher is publishing close to the set up frequency (15Hz) but I have around 2Hz on the subscriber using ros topic hz command. I am using Cyclon and changed both bashrc following the tutoria. I wasnt able to change MTU as 1500 was the limit. What could I change to increase frequency on subscriber?

 ![image](https://community.stereolabs.com/uploads/default/original/2X/a/a06ddf63b379536995b0ba767d57ac85f8d4826c.png)

 ![image](https://community.stereolabs.com/uploads/default/original/2X/e/e30914fa272148bc85d837466a0ce168aa0f9e7e.png)

![image](https://community.stereolabs.com/uploads/default/original/2X/3/36126744295221cf519b1eb70fbcf2e48c90aa91.png)

 ![image](https://community.stereolabs.com/uploads/default/original/2X/7/7dae6b01d5969642b50e1735f2cb62268b7715a9.png)

 ![image](https://community.stereolabs.com/uploads/default/original/2X/a/a06ddf63b379536995b0ba767d57ac85f8d4826c.png)

 ![image](https://community.stereolabs.com/uploads/default/original/2X/3/31d0fadde40fa65bec6f1d134345bd7010e44a7b.png)

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [June 24, 2026, 10:58am UTC](https://community.stereolabs.com/t/frequency-differences-between-recieved-and-published-images/11465/2 "2026-06-24T10:58:27Z")

</div>

Hello @Piotr.Klimaszew  
Welcome to the [StereoLabs](https://www.stereolabs.com/) community

> The publisher is publishing close to the set up frequency (15Hz) but I have around 2Hz on the subscriber using ros topic hz command.

With a 4x downscale factor the raw frame drops to roughly `480 x 270 x 4 = ~520 KB`, so at 15 Hz you are only pushing ~60 Mbit/s. That fits comfortably on a Gigabit link, so this is **not** a bandwidth problem. The bottleneck is somewhere in the DDS transport / QoS path, not the cable.

A few things to check, in order:

**1. QoS reliability mismatch on the subscriber.**  
The image topics are published with a **SENSOR\_DATA** profile (BEST\_EFFORT, volatile). If `ros2 topic hz` or your subscriber requests RELIABLE, the middleware has to retransmit, which stalls dramatically over a real network and produces exactly this kind of “publisher fast, subscriber slow” behavior. Verify with:

```auto
ros2 topic hz /zed/zed_node/rgb/image_rect_color --qos-reliability best_effort

```

If the rate jumps to ~15 Hz, the issue was a QoS mismatch in your own subscriber and you simply need to set it to BEST\_EFFORT.

**2. Confirm the rate on the Jetson side first.**  
Run `ros2 topic hz` for the same topic **locally on the Orin**. If it reads 15 Hz locally but ~2 Hz on the laptop, the loss is purely in the cross-host DDS path. If it is already low locally, the problem is upstream (grab loop / publishing) and the network is innocent.

**3. CycloneDDS fragment handling.**  
Even a downscaled image still exceeds one UDP datagram, so it is fragmented. Over a direct Ethernet link the default CycloneDDS socket buffers are often too small and dropped fragments mean the whole sample is discarded, which collapses the effective rate. Make sure your CycloneDDS XML actually applies (check `CYCLONEDDS_URI` is exported in the same shell that launches the node) and raise the receive buffer, for example:

xml

```auto
<CycloneDDS>
  <Domain>
    <Internal>
      <MinimumSocketReceiveBufferSize>10MB</MinimumSocketReceiveBufferSize>
    </Internal>
  </Domain>
</CycloneDDS>

```

You also need the matching kernel limit:

```auto
sudo sysctl -w net.core.rmem_max=10485760

```

**4. Rule out the measurement.**  
`ros2 topic hz` itself spins up a subscriber, so if it inherits a RELIABLE default or runs single-threaded under load, it can under-report. Cross-check with `ros2 topic bw` on the same topic to see whether bytes are flowing steadily.

My strong suspicion is **point 1** , a BEST\_EFFORT vs RELIABLE mismatch; that is the most common cause of this exact symptom and is independent of how much you downscale.

Network tuning and the full QoS documentation for the wrapper are here:

> **[Getting Started with ROS 2 and ZED | StereoLabs](https://www.stereolabs.com/docs/integrations/ros-2)**

Let me know the local-vs-remote `ros2 topic hz` readings and whether forcing `best_effort` changes things; that will tell us immediately which path to follow.

---

<div class="post-metadata">

**Author:** ![Piotr.Klimaszew](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/a183cd/32.png) [@Piotr.Klimaszew](https://community.stereolabs.com/u/Piotr.Klimaszew)\
**Post date:** [July 7, 2026, 11:31am UTC](https://community.stereolabs.com/t/frequency-differences-between-recieved-and-published-images/11465/3 "2026-07-07T11:31:45Z")

</div>

> [@Myzhar](#):
>
> **1. QoS reliability mismatch on the subscriber.**  
> The image topics are published with a **SENSOR\_DATA** profile (BEST\_EFFORT, volatile). If `ros2 topic hz` or your subscriber requests RELIABLE, the middleware has to retransmit, which stalls dramatically over a real network and produces exactly this kind of “publisher fast, subscriber slow” behavior. Verify with:
> 
> ```auto
> ros2 topic hz /zed/zed_node/rgb/image_rect_color --qos-reliability best_effort
> 
> ```
> 
> If the rate jumps to ~15 Hz, the issue was a QoS mismatch in your own subscriber and you simply need to set it to BEST\_EFFORT.

The frequency on the Orin correcly reads 15 Hz. I have check the QoS on both machines and it shows QoS Reliable on both of them. I am not sure how to change publisher to QoS as I dont see this as an option in .yaml files.

 ![image](https://community.stereolabs.com/uploads/default/original/2X/0/0555ae3dfe949191d8ef492772aa2e6c143fcee2.png)  
Adding this following the documentation didnt make any effect and I still have Reliable QoS