# FAILURE in sl::ERROR\_CODE after running the camera for some time

**URL:** <https://community.stereolabs.com/t/failure-in-sl-error-code-after-running-the-camera-for-some-time/9832>\
**Category:** ROS2\
**Tags:** jetson, ros2\
**Created:** [September 8, 2025, 3:52pm UTC](https://community.stereolabs.com/t/failure-in-sl-error-code-after-running-the-camera-for-some-time/9832 "2025-09-08T15:52:46Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![nino192](https://community.stereolabs.com/user_avatar/community.stereolabs.com/nino192/32/4970_2.png) [@nino192](https://community.stereolabs.com/u/nino192)\
**Post date:** [September 8, 2025, 3:52pm UTC](https://community.stereolabs.com/t/failure-in-sl-error-code-after-running-the-camera-for-some-time/9832/1 "2025-09-08T15:52:47Z")

</div>

Hi,

My setup is 2x zedXmini cameras along with ZED BOX ORIN NX 16GB. I am currently running a ros2 jazzy environment inside docker 22.04 ubuntu (jazzy installed from source). I am launching both cameras with ros2 launch zed\_wrapper zed\_camera.launch.py with camera\_name, camera\_model and serial\_number passed as their respective launch arguments. Alongside it I am running a simple static tf publisher and 2 ros2 aruco nodes.

What Im experiencing after 2-3 minutes of runtime is this error:

[component\_container\_isolated-2] [2025-09-08 13:35:49 UTC]  
[ZED][WARNING] FAILURE in sl::ERROR\_CODE sl:📷:grab(sl::RuntimeParameters)  
[component\_container\_isolated-2] [ERROR] [1757338549.141236581] [back.zed\_node]: Camera issue detected: FAILURE. Trying to recover the connection…

I have not modified the cycloneDDS.xml as per instructions, I am running this setup:

\<?xml version="1.0" encoding="UTF-8" ?\> eth0 true auto 1000 

sysctl net is configured as recommended:

net.core.rmem\_max = 2147483647  
net.ipv4.ipfrag\_time = 3  
net.ipv4.ipfrag\_high\_thresh = 134217728

Also I have noticed unusually high CPU usage and “system throttled due to overcurrent” warnings when launching the nodes.

Is there anything I can do to fix this problem? docker is already being run with runtime: nvidia and deploy:  
resources:  
reservations:  
devices:

- driver: nvidia  
count: all  
capabilities: [gpu]

Thanks in advance!

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [September 9, 2025, 12:42pm UTC](https://community.stereolabs.com/t/failure-in-sl-error-code-after-running-the-camera-for-some-time/9832/2 "2025-09-09T12:42:02Z")

</div>

Hi @nino192  
Welcome to the [StereoLabs](https://www.stereolabs.com/) community.

Are you using the latest [ZED SDK v5.0.5](https://www.stereolabs.com/developers/release) with the latest [ZED X Driver v1.3.1](https://www.stereolabs.com/developers/drivers)?