# Errors running multiple ZED X cameras using NVIDIA DeepStream

**URL:** <https://community.stereolabs.com/t/errors-running-multiple-zed-x-cameras-using-nvidia-deepstream/5162>\
**Category:** ZED X\
**Tags:** deepstream, gstreamer\
**Created:** [April 23, 2024, 11:34am UTC](https://community.stereolabs.com/t/errors-running-multiple-zed-x-cameras-using-nvidia-deepstream/5162 "2024-04-23T11:34:20Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![andrew.stringfield](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/a/a5b964/32.png) [@andrew.stringfield](https://community.stereolabs.com/u/andrew.stringfield)\
**Post date:** [April 23, 2024, 11:34am UTC](https://community.stereolabs.com/t/errors-running-multiple-zed-x-cameras-using-nvidia-deepstream/5162/1 "2024-04-23T11:34:20Z")

</div>

Hi there,

I’m trying to run a multi-camera NVIDIA DeepStream pipeline using four ZED X sensors, and I’m running into issues. This post is a follow-up to my [original post on the NVIDIA developer forums](https://forums.developer.nvidia.com/t/error-running-jetson-multicamera-pipelines-nvbuf-utils-dmabuf-fd-1-mapped-entry-not-found/290411?u=andrew.stringfield) to ask for more help.

Some system details:

- Jetson Orin NX
- ZED SDK 4.0.8
- JetPack 5.1.1

The [latest suggestion from the NVIDIA team](https://forums.developer.nvidia.com/t/error-running-jetson-multicamera-pipelines-nvbuf-utils-dmabuf-fd-1-mapped-entry-not-found/290411/9?u=andrew.stringfield) was to check the stability of the camera driver.

I understand the ZED X camera is based on an argus camera. Are the ZED X cameras designed to be useable with DeepStream/GStreamer tools, or are they only designed to work with the `zed-gstreamer` plugin tools?

If the ZED X is intended to work with DeepStream, do you have any suggestions for how I may resolve the issue described in my post on the NVIDIA dev forums?

If the ZED X is not intended to work with DeepStream, do you have examples of multi-camera systems using the `zed-gstreamer` plugins?

I appreciate any help, thanks!

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [April 23, 2024, 12:43pm UTC](https://community.stereolabs.com/t/errors-running-multiple-zed-x-cameras-using-nvidia-deepstream/5162/2 "2024-04-23T12:43:40Z")

</div>

Hi @andrew.stringfield  
Welcome to the [Stereolabs](https://www.stereolabs.com/) community.

I see a problem with your request: you cannot use four ZED X devices with the Orin NX.  
You can use four ZED X cameras only with AGX Orin.

> [@andrew.stringfield](#):
>
> I understand the ZED X camera is based on an argus camera. Are the ZED X cameras designed to be useable with DeepStream/GStreamer tools, or are they only designed to work with the `zed-gstreamer` plugin tools?

You can normally use the `zedsrc` element provided by the [zed-gstreamer](https://github.com/stereolabs/zed-gstreamer/) repository with the ZED X cameras.

> [@andrew.stringfield](#):
>
> If the ZED X is intended to work with DeepStream, do you have any suggestions for how I may resolve the issue described in my post on the NVIDIA dev forums?

If Deepstream is compatible with GStreamer elements, then you can use it.

> [@andrew.stringfield](#):
>
> If the ZED X is not intended to work with DeepStream, do you have examples of multi-camera systems using the `zed-gstreamer` plugins?

There are no ready examples, but you can normally design a multi-src pipeline based on `zedsrc` elements. It’s only important that you set the `camera-sn` of each element to correctly assign them to the correct camera.