# Error building ZED ROS2 wrapper on JetPack 6.0.0 with NVIDIA ROS Isaac 3.1

**URL:** <https://community.stereolabs.com/t/error-building-zed-ros2-wrapper-on-jetpack-6-0-0-with-nvidia-ros-isaac-3-1/11323>\
**Category:** ROS2\
**Tags:** jetson, ros2\
**Created:** [May 18, 2026, 6:29am UTC](https://community.stereolabs.com/t/error-building-zed-ros2-wrapper-on-jetpack-6-0-0-with-nvidia-ros-isaac-3-1/11323 "2026-05-18T06:29:40Z")\
**Posts on this page:** 3\
**Page:** 1

<div class="post-metadata">

**Author:** ![andrew.stringfield](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/a/a5b964/32.png) [@andrew.stringfield](https://community.stereolabs.com/u/andrew.stringfield)\
**Post date:** [May 18, 2026, 6:29am UTC](https://community.stereolabs.com/t/error-building-zed-ros2-wrapper-on-jetpack-6-0-0-with-nvidia-ros-isaac-3-1/11323/1 "2026-05-18T06:29:40Z")

</div>

Hi there,

I’m working on getting ZED ROS2 nodes running with 4 ZED X cameras and NTROS enabled on a Jetpack 6.0.0 system, following these instructions:

> **[Setting up Isaac™ ROS to work with ZED Cameras in ROS 2 - Stereolabs](https://www.stereolabs.com/docs/isaac-ros/setting_up_isaac_ros)**
>
> This guide will help you set up the NVIDIA® Isaac™ ROS packages to work with the ZED ROS 2 Wrapper.

Since I’m using JetPack 6.0.0, I’m using Isaac ROS 3.1 instead of 3.2 as specified in the instructions:

```bash
git clone --branch release-3.1 https://github.com/NVIDIA-ISAAC-ROS/isaac_ros_common.git --recurse-submodules1

```

Since I’m using ZED SDK 5.0.5, I’ve also cloned the corresponding `zed-ros2-wrapper` version:

```bash
 git clone --branch humble-v5.0.0 https://github.com/stereolabs/zed-ros2-wrapper.git

```

However, when building the `zed_wrapper` ROS2 package, I see this error:

```bash
admin@nvidia-desktop:/workspaces/isaac_ros-dev$ colcon build --symlink-install --cmake-args=-DCMAKE_BUILD_TYPE=Release --packages-up-to zed_wrapper
Starting >>> zed_components
[Processing: zed_components]                             
[Processing: zed_components]                                     
--- stderr: zed_components                                       
 * ISAAC ROS Nitros transport is available
/workspaces/isaac_ros-dev/src/zed-ros2-wrapper/zed_components/src/zed_camera/src/zed_camera_component_main.cpp: In member function ‘void stereolabs::ZedCamera::callback_setRoi(std::shared_ptr<rmw_request_id_s>, std::shared_ptr<zed_msgs::srv::SetROI_Request_<std::allocator<void> > >, std::shared_ptr<zed_msgs::srv::SetROI_Response_<std::allocator<void> > >)’:
/workspaces/isaac_ros-dev/src/zed-ros2-wrapper/zed_components/src/zed_camera/src/zed_camera_component_main.cpp:8063:40: error: ‘NitrosDiagnosticsConfig’ is not a member of ‘nvidia::isaac_ros::nitros’; did you mean ‘NitrosStatisticsConfig’?
 8063 | nvidia::isaac_ros::nitros::NitrosDiagnosticsConfig(), mQos);
      | ^ ~~~~~~~~~~~~~~~~~~~~~~
      | NitrosStatisticsConfig
/workspaces/isaac_ros-dev/src/zed-ros2-wrapper/zed_components/src/zed_camera/src/zed_camera_component_video_depth.cpp: In lambda function:
/workspaces/isaac_ros-dev/src/zed-ros2-wrapper/zed_components/src/zed_camera/src/zed_camera_component_video_depth.cpp:177:38: error: ‘NitrosDiagnosticsConfig’ is not a member of ‘nvidia::isaac_ros::nitros’; did you mean ‘NitrosStatisticsConfig’?
  177 | nvidia::isaac_ros::nitros::NitrosDiagnosticsConfig(), mQos);
      | ^ ~~~~~~~~~~~~~~~~~~~~~~
      | NitrosStatisticsConfig
/workspaces/isaac_ros-dev/src/zed-ros2-wrapper/zed_components/src/zed_camera/src/zed_camera_component_video_depth.cpp: In member function ‘void stereolabs::ZedCamera::initVideoDepthPublishers()’:
/workspaces/isaac_ros-dev/src/zed-ros2-wrapper/zed_components/src/zed_camera/src/zed_camera_component_video_depth.cpp:201:34: error: ‘NitrosDiagnosticsConfig’ is not a member of ‘nvidia::isaac_ros::nitros’; did you mean ‘NitrosStatisticsConfig’?
  201 | nvidia::isaac_ros::nitros::NitrosDiagnosticsConfig(), mQos);
      | ^ ~~~~~~~~~~~~~~~~~~~~~~
      | NitrosStatisticsConfig
gmake[2]: *** [CMakeFiles/zed_camera_component.dir/build.make:146: CMakeFiles/zed_camera_component.dir/src/zed_camera/src/zed_camera_component_video_depth.cpp.o] Error 1
gmake[2]: *** Waiting for unfinished jobs....
gmake[2]: *** [CMakeFiles/zed_camera_component.dir/build.make:132: CMakeFiles/zed_camera_component.dir/src/zed_camera/src/zed_camera_component_main.cpp.o] Error 1
gmake[1]: *** [CMakeFiles/Makefile2:166: CMakeFiles/zed_camera_component.dir/all] Error 2
gmake[1]: *** Waiting for unfinished jobs....
gmake: *** [Makefile:146: all] Error 2
---
Failed <<< zed_components [1min 2s, exited with code 2]

Summary: 0 packages finished [1min 3s]
  1 package failed: zed_components
  1 package had stderr output: zed_components
  1 package not processed

```

Looking at the [isaac\_ros\_nitros](https://github.com/NVIDIA-ISAAC-ROS/isaac_ros_nitros/blob/v3.2-1/isaac_ros_nitros/include/isaac_ros_nitros/nitros_publisher_subscriber_base.hpp) repo, it seems that the member name was changed between `v3.1.0` and `3.2.1`:

- `v3.1.0` → `NitrosStatisticsConfig`
- `v3.2.1` → `NitrosDiagnosticsConfig`

Since NITROS support was added in `zed-ros2-wrapper` version [`humble-v5.0.0`](https://github.com/stereolabs/zed-ros2-wrapper/releases/tag/humble-v5.0.0), referencing the `NitrosDiagnosticsConfig` member, it seems that the `zed-ros2-wrapper` **isn’t compatible with Isaac ROS2 versions earlier than 3.2**.

**Question 1** : Is this intentional, or is it just a bug?

I assume it’s just a bug since [this section of the setup instructions](https://www.stereolabs.com/docs/isaac-ros/setting_up_isaac_ros#configure-nvidia-isaac-ros-using-docker-with-zed-cameras) implies that JetPack 6.0.0 (and hence Isaac ROS 3.1) is supported:

> If you are using a different version of the JetPack SDK, you must adjust the URL accordingly. For example, if you are using JetPack 6.0, you must change `l4t36.4` to `l4t36.3`.

I’ve also been able to build the `zed_wrapper` package on this system and get the camera nodes running by changing the references from `NitrosStatisticsConfig` to `NitrosDiagnosticsConfig`.

**Question 2** : Is the ZED ROS2 w/ NITROS integration expected to work with Jetpack 6.0.0 and Isaac ROS 3.1 systems? If so, are there any caveats to working with this configuration, or should it be fully supported?

Thanks in advance!

## System Overview

- **Platform** : Syslogic RML A4NX (GMSL)
- **JetPack** : 6.0.0
- **Cameras** : 4x ZED X cameras
- **ZED SDK** : 5.0.5
- **Drivers** : 1.3.0

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [May 18, 2026, 8:15am UTC](https://community.stereolabs.com/t/error-building-zed-ros2-wrapper-on-jetpack-6-0-0-with-nvidia-ros-isaac-3-1/11323/2 "2026-05-18T08:15:23Z")

</div>

Hi @andrew.stringfield

> [@andrew.stringfield](#):
>
> **Question 1** : Is this intentional, or is it just a bug?

NITROS support was introduced in `zed-ros2-wrapper humble-v5.0.0` against the Isaac ROS 3.2 API. The struct was renamed from `NitrosStatisticsConfig` (v3.1) to `NitrosDiagnosticsConfig` (v3.2) by NVIDIA, and we built against the new name. The wrapper is currently only compatible with Isaac ROS 3.2.x — this is documented on our [Isaac ROS integration page](https://www.stereolabs.com/docs/isaac-ros), but I agree it’s not as prominent as it should be on the setup guide itself. I’ll flag it internally.

Support for Isaac ROS 4.x (JetPack 7 / Jetson Thor) is planned for a future release.

> [@andrew.stringfield](#):
>
> **Question 2** : Is the ZED ROS2 w/ NITROS integration expected to work with Jetpack 6.0.0 and Isaac ROS 3.1 systems? If so, are there any caveats to working with this configuration, or should it be fully supported?

The note you quoted about adjusting `l4t36.4` → `l4t36.3` only refers to the **ZED SDK installer URL** , not to the Isaac ROS version. It’s there because the ZED SDK ships separate L4T-specific binaries. The supported path for the wrapper with NITROS is JetPack 6.1+ with Isaac ROS 3.2.x — JetPack 6.0 is below the floor NVIDIA set for Isaac ROS 3.2.

I’ll make sure this prerequisite is called out more clearly in the setup guide.

**About your workaround**

Renaming the symbol back to `NitrosStatisticsConfig` builds, but I’d be cautious about relying on it in production. The wrapper currently default-constructs the config (`NitrosDiagnosticsConfig()`) without setting fields, so you’ll likely get a working build — but the two structs are not field-compatible across the rename, and the diagnostics behavior may silently differ. Given that you’ve been chasing the 5 Hz / 30 Hz instability on this same platform, I’d rather you weren’t also debugging on a patched diagnostics path.

**Recommended options, in order**

1. **Upgrade to JetPack 6.1+ and use Isaac ROS 3.2.x.** This is the configuration we test against. Worth checking with Syslogic first whether their BSP for the RML A4NX supports JP 6.1 or 6.2.
2. **If JP 6.1 is blocked by the BSP** , fall back to a pre-NITROS wrapper tag (anything before `humble-v5.0.0`). You lose NITROS acceleration but you get a tested build on your current stack. With 4× ZED X at 30 Hz this is a measurable performance hit, so option 1 is preferable when feasible.
3. **Keep your local patch** only as a short-term unblock while you work toward option 1.

Let me know which path makes sense for your setup, and if you do go the BSP-upgrade route, I’m happy to help debug if anything breaks on the wrapper side.

---

<div class="post-metadata">

**Author:** ![andrew.stringfield](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/a/a5b964/32.png) [@andrew.stringfield](https://community.stereolabs.com/u/andrew.stringfield)\
**Post date:** [June 4, 2026, 2:51am UTC](https://community.stereolabs.com/t/error-building-zed-ros2-wrapper-on-jetpack-6-0-0-with-nvidia-ros-isaac-3-1/11323/3 "2026-06-04T02:51:40Z")

</div>

@Myzhar thank you for your detailed response.

We’ve taken Option 2 from your list and are trying to run a mutli-ZED X ROS2 node using Isaac ROS 3.1 and ZED Wrapper `humble-v4.2.5`.

We’re having issues getting the node to run reliably, and would greatly appreciate your help debugging them.

I’ve made a separate post on the forums here:

> [@Multi-ZED X ROS2 node repeatedly crashes on JetPack 6.0.0 with Isaac ROS 3.1](https://community.stereolabs.com/t/multi-zed-x-ros2-node-repeatedly-crashes-on-jetpack-6-0-0-with-isaac-ros-3-1/11399):
>
> Summary We’re running 4× ZED X cameras via GMSL using the zed\_multi\_camera ROS2 node inside an Isaac ROS Docker container on Jetson Orin NX (Syslogic IPC). The node consistently crashes after a period of time — cameras enter CAMERA\_REBOOTING, fail to recover, and eventually one camera returns FAILURE, taking down the whole node. We’ve tested across two different machines, and with multiple ZED SDK versions — the crash is 100% reproducible. We’d like support to understand how we can make a mulit…