# Dual ZED X on ZED Box Duo: repeatable Argus AlreadyAllocated and InvalidState despite two working streams (SDK 5.4.1, driver 1.4.3)

**URL:** <https://community.stereolabs.com/t/dual-zed-x-on-zed-box-duo-repeatable-argus-alreadyallocated-and-invalidstate-despite-two-working-streams-sdk-5-4-1-driver-1-4-3/11668>\
**Category:** ROS2\
**Created:** [August 26, 2026, 8:44am UTC](https://community.stereolabs.com/t/dual-zed-x-on-zed-box-duo-repeatable-argus-alreadyallocated-and-invalidstate-despite-two-working-streams-sdk-5-4-1-driver-1-4-3/11668 "2026-08-26T08:44:39Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![payk](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/90ced4/32.png) [@payk](https://community.stereolabs.com/u/payk)\
**Post date:** [August 26, 2026, 8:44am UTC](https://community.stereolabs.com/t/dual-zed-x-on-zed-box-duo-repeatable-argus-alreadyallocated-and-invalidstate-despite-two-working-streams-sdk-5-4-1-driver-1-4-3/11668/1 "2026-08-26T08:44:40Z")

</div>

Hello [Stereolabs](https://www.stereolabs.com/) team,

we are testing two ZED X cameras connected to one ZED Box Duo. Both cameras  
can be opened and streamed at the same time, but `nvargus-daemon` emits  
repeatable resource and state errors during every dual-camera startup.

The sender is a native application, not a Docker container. A single process  
owns two `sl::Camera` instances. It opens the cameras sequentially with  
`setFromGMSLPort()`, waits two seconds between opens, verifies the expected  
serial number after each open, and enables both H.265 encoders only after both  
cameras have opened successfully.

There is no camera hotplug and neither `nvargus-daemon` nor `zed_x_daemon` is  
restarted while a camera session is open. Both cameras are connected before  
boot. The sender and receiver processes stop cleanly after each test.

### Sender environment

- [Stereolabs](https://www.stereolabs.com/) ZED Box Duo, Jetson Orin NX 16 GB
- JetPack 6.2.1
- L4T 36.4.4
- Kernel 5.15.148-tegra
- ZED SDK 5.4.1
- `stereolabs-zedbox-duo`  
`1.4.3-LI-MAX96712-ZEDBOX-L4T36.4.0`
- Two ZED X cameras, firmware 2001, on GMSL ports 0 and 1
- HD1200 at 30 FPS, H.265, 12.5 Mbit/s per camera
- `DEPTH_MODE::NONE` on the sender

The system was upgraded from ZED SDK 5.2.3 and ZED Box Duo driver 1.4.1 to  
SDK 5.4.1 and driver 1.4.3. The upgrade removed the previous  
`Failed to connect to zed_x_daemon` warning from the single-process test, but  
the Argus messages below remain.

### Receiver and functional result

The two network streams are received by a Jetson AGX Orin running ZED SDK  
5.4.1 and two ROS 2 wrapper instances. Both A/B runs passed all ten checked  
data paths for the two cameras: RGB, registered depth, reduced point cloud,  
health, and heartbeat. Point clouds remained close to the configured 5 Hz  
target. Both sender streams and both receivers shut down with exit code 0.

### Reproduction

1. Boot the ZED Box with both cameras already connected.
2. Confirm that both cameras are `AVAILABLE` and that `zed_x_daemon` is active.
3. Start the single-process sender with open order `cam0-first`.
4. Open port 0, wait two seconds, open port 1, verify both serial numbers, and  
then enable both streams.
5. Start both network receivers and verify the ten ROS 2 data paths.
6. Stop sender and receivers cleanly.
7. Repeat with open order `cam1-first`.
8. Inspect the isolated `nvargus-daemon` journal windows.

### Results

| Run | Open order | All 10 receiver paths | Point cloud cam0/cam1 | AlreadyAllocated | NvCameraUtils InvalidState | Wrong frequency range | ModuleNotPresent | Failed to connect to zed\_x\_daemon |
| --- | --- | --- | --- | --- | --- | --- | --- | --- |
| A | cam0-first | passed | 5.09 / 5.19 Hz | 12 | 8 | 531 | 60 | 0 |
| B | cam1-first | passed | 5.74 / 5.00 Hz | 12 | 4 | 357 | 30 | 0 |

Run A contains one additional `ZED_Explorer` provider cycle immediately before  
the sender starts. It accounts for 30 of the 60 `ModuleNotPresent` messages.  
The `Wrong frequency range` rate is approximately 5.5 messages/s in run A and  
5.3 messages/s in run B, so the difference in raw totals is caused mainly by  
the different run durations.

Representative messages are:

```plaintext
(Argus) Error AlreadyAllocated: Device 0 (of 1) is in use
(NvCameraUtils) Error InvalidState: Mutex not initialized
(NvCameraUtils) Error InvalidState: Mutex has not been initialized
(NvCamV4l2) Error ModuleNotPresent: V4L2Device not available
SCF: Error BadParameter: Sensor could not be opened.
Wrong frequency range!

```

We found the existing community statement that `Wrong frequency range!` can  
be ignored if the cameras work normally. We therefore do not treat that  
warning alone as proof of a failed stream. Our main concern is the repeatable  
`AlreadyAllocated` and uninitialized-mutex `InvalidState` combination during a  
clean two-camera open on the already recommended SDK 5.4.1 / driver 1.4.3  
stack.

### Questions

1. Is using two `sl::Camera` instances in one native process supported for two  
ZED X cameras on this ZED Box Duo stack?
2. Are `AlreadyAllocated` and the uninitialized-mutex `NvCameraUtils InvalidState` messages expected internal enumeration/probing messages, or  
do they indicate a driver or Argus defect?
3. Can this state affect long-term stability, frame timing, hardware sync, or  
later camera recovery even though both short streams remain functional?
4. Are the `ModuleNotPresent` and `BadParameter` messages expected probes for  
unused device-tree modules on this carrier configuration?
5. Is there a recommended open order, minimum delay, sync configuration, or  
newer compatible driver for JetPack 6.2.1 / L4T 36.4.4?
6. Which messages may safely be excluded from a production health gate, and  
which ones should still be treated as a camera-stack fault?

I have attached sanitized A/B sender logs, isolated `nvargus-daemon` logs, a  
test report with exact counts, and a fresh `ZED_Diagnostic_Results.json`.

Related discussions already checked:

- [https://community.stereolabs.com/t/zed-x-grab-stuck-in-failure-after-argus-zed-x-daemon-failure/11590](https://community.stereolabs.com/t/zed-x-grab-stuck-in-failure-after-argus-zed-x-daemon-failure/11590)
- [https://community.stereolabs.com/t/zed-x-camera-error-camera-rebooting-argus-error-fileoperationfailed-invalidstate/10558](https://community.stereolabs.com/t/zed-x-camera-error-camera-rebooting-argus-error-fileoperationfailed-invalidstate/10558)
- [https://community.stereolabs.com/t/nvargus-daemon-have-some-error-wrong-frequency-range/10486](https://community.stereolabs.com/t/nvargus-daemon-have-some-error-wrong-frequency-range/10486)
- [https://community.stereolabs.com/t/opening-multiple-zed-x-by-serial-number-appears-to-be-unreliable/6689](https://community.stereolabs.com/t/opening-multiple-zed-x-by-serial-number-appears-to-be-unreliable/6689)

Thank you for checking whether these messages are benign for this exact stack  
or whether an additional driver fix or configuration change is required.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [August 27, 2026, 1:49pm UTC](https://community.stereolabs.com/t/dual-zed-x-on-zed-box-duo-repeatable-argus-alreadyallocated-and-invalidstate-despite-two-working-streams-sdk-5-4-1-driver-1-4-3/11668/2 "2026-08-27T13:49:45Z")

</div>

Hi @payk  
Welcome to the [StereoLabs](https://www.stereolabs.com/) community.

Thank you for a genuinely well built report; the A/B structure, the isolated `nvargus-daemon` windows, and the per message counts make this much faster to analyze than the usual log dump.

One general remark first, because it frames most of the individual answers. Every message in your list is emitted by the NVIDIA Argus stack (`nvargus-daemon`, `NvCameraUtils`, `NvCamV4l2`, `SCF`), not by the ZED SDK and not by the ZED X Driver. Argus prints a large part of its enumeration and probing activity at “Error” severity even when the operation that follows completes correctly, so severity in the journal is not a reliable fault indicator. Your own numbers support the benign interpretation: 12 `AlreadyAllocated` in both runs, identical and independent of open order and of run duration, and `ModuleNotPresent` in exact multiples of 30 per provider cycle. Those are fixed size probe loops, not a race and not a leak.

> 1. Is using two `sl::Camera` instances in one native process supported for two ZED X cameras on this ZED Box Duo stack?

Yes, fully supported, and it is the configuration we recommend on a single Jetson for two [ZED X](https://www.stereolabs.com/store/products/zed-x-stereo-camera) cameras. The two requirements are that each `sl::Camera` object is grabbed from its own thread, and that the `open()` calls are serialized rather than concurrent; you are already doing both. Reference: [Hardware Recommendations for GMSL2 cameras](https://docs.stereolabs.com/docs/development/zed-sdk/modules/camera/multi-camera#hardware-recommendations-for-gmsl2-cameras).

> 1. Are `AlreadyAllocated` and the uninitialized-mutex `NvCameraUtils InvalidState` messages expected internal enumeration/probing messages, or do they indicate a driver or Argus defect?

They are expected probing and teardown messages, not a defect. `AlreadyAllocated: Device 0 (of 1) is in use` is printed when an Argus client queries a sensor device that is already owned by a live capture session, which is unavoidable when the SDK enumerates devices while the first camera is already streaming; the uninitialized mutex `InvalidState` lines come from the destruction of those short lived probing contexts, where the mutex was never created because the probe did not reach that stage.

> 1. Can this state affect long-term stability, frame timing, hardware sync, or later camera recovery even though both short streams remain functional?

No. These messages are confined to the enumeration and open window and do not recur once both sessions are streaming, so nothing accumulates with uptime. Frame synchronization between the two ports is done by the hardware trigger generated on the carrier board, completely independent of Argus client side device arbitration, so it is not affected either; see [Frame synchronization](https://docs.stereolabs.com/docs/development/zed-sdk/modules/camera/multi-camera#frame-synchronization).

> 1. Are the `ModuleNotPresent` and `BadParameter` messages expected probes for unused device-tree modules on this carrier configuration?

Yes. The device tree shipped with the driver package declares all the ports supported by the MAX96712 deserializer, so Argus probes the nodes of the ports with no camera attached; `V4L2Device not available` and `SCF: Error BadParameter: Sensor could not be opened.` are the expected outcome of those probes. Your count of 30 per provider cycle, invariant with respect to open order, is exactly the signature of that fixed probe over the unpopulated nodes.

> 1. Is there a recommended open order, minimum delay, sync configuration, or newer compatible driver for JetPack 6.2.1 / L4T 36.4.4?

There is no recommended open order; the ports are symmetric, and your A/B result confirms it. Once `open()` has returned `SUCCESS` the device is fully acquired, so no additional delay is formally required; your two seconds are conservative and can be reduced if boot to stream time matters, keeping the calls strictly sequential. The `1.4.3-LI-MAX96712-ZEDBOX-L4T36.4.0` package is the correct one for the JetPack 6.2.x line, and I recommend checking the [ZED X Driver download page](https://www.stereolabs.com/developers/drivers) from time to time, since new versions are published there.

> 1. Which messages may safely be excluded from a production health gate, and which ones should still be treated as a camera-stack fault?

I would exclude from the gate: `Wrong frequency range!`, `ModuleNotPresent: V4L2Device not available`, `SCF: Error BadParameter: Sensor could not be opened.`, and `AlreadyAllocated` plus `NvCameraUtils InvalidState` when they fall inside the open window. I would treat as a fault: those same messages appearing after both cameras are streaming, `Argus Error FileOperationFailed`, any camera reboot notification, `Failed to connect to zed_x_daemon`, and any `grab()` return different from `ERROR_CODE::SUCCESS`. My suggestion, though, is not to build the gate on the journal at all, but on the SDK side signals, which are the actual contract: the `grab()` return code, image timestamp continuity, and the [Health Status](https://docs.stereolabs.com/docs/tutorials/health-status) module, which is designed exactly for this kind of production monitoring.

So, to summarize: on SDK 5.4.1 with driver 1.4.3 what you observe is normal Argus verbosity for a dual camera open, and the fact that both runs passed all ten data paths with clean exit codes is the meaningful result. If at some point the pattern changes, in particular counts growing with runtime or any of those messages appearing during streaming rather than at open, please post the new `nvargus-daemon` window and we will look into it, because that would be a different signature from the one described here.