# Different ZED X framesrates across different Jetson machines

**URL:** <https://community.stereolabs.com/t/different-zed-x-framesrates-across-different-jetson-machines/6898>\
**Category:** ZED X\
**Tags:** python, jetson\
**Created:** [August 27, 2024, 1:48am UTC](https://community.stereolabs.com/t/different-zed-x-framesrates-across-different-jetson-machines/6898 "2024-08-27T01:48:21Z")\
**Posts on this page:** 8\
**Page:** 1

<div class="post-metadata">

**Author:** ![andrew.stringfield](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/a/a5b964/32.png) [@andrew.stringfield](https://community.stereolabs.com/u/andrew.stringfield)\
**Post date:** [August 27, 2024, 1:48am UTC](https://community.stereolabs.com/t/different-zed-x-framesrates-across-different-jetson-machines/6898/1 "2024-08-27T01:48:21Z")

</div>

I have two jetson machines running systems that record data from multiple ZED X cameras.

On Machine 1, the framerate according to `get_current_fps()` is consistently 13-15 FPS, while on Machine 2 the framerate is consistently 9-11 FPS.

Machine 1 is using four cameras while Machine 2 has only three, so I’d expect the framerate to be higher on Machine 2.

The compute hardware is identical, both are:

> **[Rugged Computer RPC RML A4NX (GMSL)](https://www.syslogic.com/jetson-orin-nx/rugged-computer-rpc-rml-a4nx-gmsl)**
>
> The Rugged Computer RML A3 is IP67 rated. Syslogic combines the NVIDIA Jetson module with its own carrier board to meet high shock and vibration requirements.

Both systems are running identical code in a Docker image, and the ZED SDK version is the same, `4.1.3.`

Could you give me some advice for other troubleshooting steps I could to uncover the cause of the discrepancy in framerates?

Any help is greatly appreciated.

Thanks!

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [August 27, 2024, 10:09am UTC](https://community.stereolabs.com/t/different-zed-x-framesrates-across-different-jetson-machines/6898/2 "2024-08-27T10:09:45Z")

</div>

Hi @andrew.stringfield  
we are testing this behavior internally and will get back to you as soon as possible.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [August 27, 2024, 10:31am UTC](https://community.stereolabs.com/t/different-zed-x-framesrates-across-different-jetson-machines/6898/3 "2024-08-27T10:31:07Z")

</div>

@andrew.stringfield can you confirm that you are using the same power mode (`nvpmodel`) on both devices?

---

<div class="post-metadata">

**Author:** ![andrew.stringfield](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/a/a5b964/32.png) [@andrew.stringfield](https://community.stereolabs.com/u/andrew.stringfield)\
**Post date:** [August 29, 2024, 5:26am UTC](https://community.stereolabs.com/t/different-zed-x-framesrates-across-different-jetson-machines/6898/4 "2024-08-29T05:26:38Z")

</div>

@Myzhar yes, both machines are operating in `MAXN` power mode.

When I look at the journal logs while the recording application is running, I’m seeing the following Argus error a lot:

```bash
Aug 29 15:18:43 collection-2 nvargus-daemon[1168]: (Argus) Error AlreadyAllocated: Device 0 (of 1) is in use (in src/api/CameraProviderImpl.cpp, function createCaptureSessionInternal(), line 272)

```

- On Machine 1, the error appears every now and then - every 30 seconds or so
- On Machine 2, the error is logged constantly - several times per second

Could this be linked to the issue?

Thanks!

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [August 29, 2024, 7:26am UTC](https://community.stereolabs.com/t/different-zed-x-framesrates-across-different-jetson-machines/6898/5 "2024-08-29T07:26:30Z")

</div>

This can be a piece of useful information.  
Can you confirm that the configuration is identical?  
Same cable length, same GMSL2 ports, etc.

---

<div class="post-metadata">

**Author:** ![andrew.stringfield](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/a/a5b964/32.png) [@andrew.stringfield](https://community.stereolabs.com/u/andrew.stringfield)\
**Post date:** [August 29, 2024, 11:44pm UTC](https://community.stereolabs.com/t/different-zed-x-framesrates-across-different-jetson-machines/6898/6 "2024-08-29T23:44:23Z")

</div>

@Myzhar sure thing, config is as follows:

**Machine 1**

- 3x ZED X connected to GMSL ports 2, 4 and 5 using 1.5-metre cables
- 1x ZED X connected to GMSL port 7 using a 5-metre cable

**Machine 2**

- 3x ZED X connected to GMSL ports 2, 4 and 5 using 1.5m cables

The configuration is the same for both machines, with Machine 1 having an additional camera connected via a 5-metre cable.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [September 9, 2024, 9:50am UTC](https://community.stereolabs.com/t/different-zed-x-framesrates-across-different-jetson-machines/6898/7 "2024-09-09T09:50:43Z")

</div>

Hi @andrew.stringfield  
we are trying to replicate your configuration to find a reason to the behavi or that you described.  
Can you please run the command `sudo ZED_Diagnostic --dmesg` and send the report file to [support@stereolabs.com](mailto:support@stereolabs.com)?

---

<div class="post-metadata">

**Author:** ![andrew.stringfield](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/a/a5b964/32.png) [@andrew.stringfield](https://community.stereolabs.com/u/andrew.stringfield)\
**Post date:** [September 16, 2024, 3:54am UTC](https://community.stereolabs.com/t/different-zed-x-framesrates-across-different-jetson-machines/6898/8 "2024-09-16T03:54:04Z")

</div>

@Myzhar I’ve generated a log and emailed to support, thanks. The diagnostic was run inside the Docker container.

I realised that both containers are actually running ZED SDK 4.0.8, not 4.1.3.

However, I’ve confirmed that the containers on both Machine 1 and Machine 2 are still running the same SDK version.

Thanks!