# Depth-based “humanoid” mask, feet-vs-floor separation issues

**URL:** <https://community.stereolabs.com/t/depth-based-humanoid-mask-feet-vs-floor-separation-issues/9879>\
**Category:** Unity\
**Tags:** sdk, zed-sdk, depth, unity\
**Created:** [September 15, 2025, 9:50am UTC](https://community.stereolabs.com/t/depth-based-humanoid-mask-feet-vs-floor-separation-issues/9879 "2025-09-15T09:50:56Z")\
**Posts on this page:** 4\
**Page:** 1

<div class="post-metadata">

**Author:** ![Jeff](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/j/e19b73/32.png) [@Jeff](https://community.stereolabs.com/u/Jeff)\
**Post date:** [September 15, 2025, 9:50am UTC](https://community.stereolabs.com/t/depth-based-humanoid-mask-feet-vs-floor-separation-issues/9879/1 "2025-09-15T09:50:56Z")

</div>

## Context

- **Unity** 6000.0.33, **URP**

- **ZED Unity SDK** 5.0.1

- I render a **humanoid mask** in a custom shader using **depth**. The RGB image is cropped by distance **and** I subtract the **floor** using a one-shot **Y-height** calibration (from `MEASURE.XYZ`) to keep the feet while removing the floor.

- **Attached screenshot** : either the mask stops around the ankles, or, if I widen the band, feet are included but so is the floor and nearby objects.

- **Camera** : ZED 2 / ZED 2i

- **Depth mode** : Neural Depth Mode

## Current results

1. Narrow band → mask **cuts at the ankles**.

 ![image](https://community.stereolabs.com/uploads/default/original/2X/5/58e569a65d190932a287fc52310197252c24ae75.jpeg)

1. Wider band (`floorHeightBandMeters`) → **feet included better** , but **floor starts to leak**.

 ![image](https://community.stereolabs.com/uploads/default/original/2X/b/bc0c976c7cba183502222d81e4909c447df22194.jpeg)

1. Even wider band → **floor and floor objects** included.

 ![image](https://community.stereolabs.com/uploads/default/original/2X/e/e5d3742686e497462a9c00c2fee80a839e7211c5.jpeg)

## Implementation (short)

1. Full-screen `Graphics.Blit` into a `RenderTexture` with **Custom/ZEDMask**.
2. **Runtime** mask uses `MEASURE.DEPTH`.
3. **Floor calibration** uses `MEASURE.XYZ`; I take **Y (meters)** to build a “Floor” `RenderTexture` that I subtract in the shader.
4. Key knob: `floorHeightBandMeters` (tolerance around floor height).

## Minimal C# excerpt (param passing)

> public void CalibrateFloor()  
> {  
> Texture rgb = zedPlane?.TextureEye;  
> if (rgb == null || maskMaterial == null) return;
> 
> ```auto
> Texture xyzTex = zedCamera != null
> ? zedCamera.CreateTextureMeasureType(sl.MEASURE.XYZ)
> : zedPlane?.Depth; 
> if (xyzTex == null) return;
> 
> int w = rgb.width, h = rgb.height;
> if (floorRT == null || floorRT.width != w || floorRT.height != h)
> {
> if (floorRT != null) floorRT.Release();
> floorRT = new RenderTexture(w, h, 0, RenderTextureFormat.ARGB32);
> floorRT.Create();
> }
> 
> maskMaterial.SetFloat("_HasFloor", 0f);
> maskMaterial.SetTexture("_FloorTex", Texture2D.blackTexture);
> 
> maskMaterial.SetTexture("_DepthTex", xyzTex);  
> maskMaterial.SetFloat("_UseYFloor", 1f);
> maskMaterial.SetFloat("_FloorY", floorHeightMeters);
> maskMaterial.SetFloat("_FloorYBand", floorHeightBandMeters);
> maskMaterial.SetFloat("_BuildFloor", 1f);
> 
> Graphics.Blit(rgb, floorRT, maskMaterial);
> 
> maskMaterial.SetFloat("_BuildFloor", 0f);
> floorReady = true;
> 
> ```
> 
> }

## Minimal C# Shader

> // — Build floor mode: mark floor pixels (Y close to \_FloorY) —  
> if (\_BuildFloor \> 0.5)  
> {  
> float3 P = depth.rgb; // XYZ in meters (camera space)  
> if (all(P == 0)) return half4(0,0,0,1);
> 
> ```auto
> float dy = abs(P.y - _FloorY);
> float isFloor = step(dy, _FloorYBand);
> 
> return half4(isFloor, isFloor, isFloor, 1);
> 
> ```
> 
> }
> 
> // — Runtime: combine mask and floor subtraction —  
> float4 maskRaw = SAMPLE\_TEXTURE2D(\_MaskTex, sampler\_MaskTex, uv);  
> float4 maskCol = float4(maskRaw.b, maskRaw.g, maskRaw.r, maskRaw.a);

## **Works**

- Distance-based mask ✅

- Y-based floor subtraction ✅ (generally)

- Feet vs floor ❌

## **Issue**

- **Feet vs floor boundary** is unstable: either **ankles get cut** , or **floor leaks** into the mask when widening the band.

## **Tried**

- `floorHeightBandMeters` **0.02–0.08 m**

- **Floor normal** dot thresholding

## **Questions**

I currently build a **floor mask** from a **Y-band** (`MEASURE.XYZ`) and **subtract** it from a **DEPTH-based** humanoid mask.

- **Is there a better way** to make the **feet vs floor** split more robust?
- Is `MEASURE.XYZ` **Y** strictly in **camera space** (roll-independent), or should I transform **camera→world** to stabilize floor height?

---

<div class="post-metadata">

**Author:** ![BenjaminV](https://community.stereolabs.com/user_avatar/community.stereolabs.com/benjaminv/32/3863_2.png) [@BenjaminV](https://community.stereolabs.com/u/BenjaminV)\
**Post date:** [September 15, 2025, 12:04pm UTC](https://community.stereolabs.com/t/depth-based-humanoid-mask-feet-vs-floor-separation-issues/9879/2 "2025-09-15T12:04:28Z")

</div>

Hi,  
If you know the camera’s height in advance, you can also set it directly to avoid any estimation inaccuracy when performed by the ZED SDK.

Also, I’d recommend setting “tracking is static” to true (see image). With this option enabled, the camera’s position is estimated once (same as your floor subtraction).

 ![image](https://community.stereolabs.com/uploads/default/original/2X/7/72e7662d89d06a7ad465a877b84788d3816924f2.png)

Yes, the depth is in Camera space, you might want to transform it to world space (you can use `zedManager.GetZedRootTransform().TransformPoint()`).

---

<div class="post-metadata">

**Author:** ![Jeff](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/j/e19b73/32.png) [@Jeff](https://community.stereolabs.com/u/Jeff)\
**Post date:** [September 15, 2025, 3:09pm UTC](https://community.stereolabs.com/t/depth-based-humanoid-mask-feet-vs-floor-separation-issues/9879/3 "2025-09-15T15:09:44Z")

</div>

Hello, and thank you for the quick answer !

I’ve enabled Tracking is static. I did not express myself clearly; My issue isn’t pose stability, but the stability boundary between the feet and the floor in the mask.

What I’m doing now:

- Build a foreground mask from depth (range-based).
- Build a floor mask once from MEASURE.XYZ in a low ROI by marking pixels whose Y is near Y0.
- Subtract the floor mask from the foreground mask.

Outcome: with a narrow Y band I lose the ankles; if I widen the band, the floor starts leaking (and floor objects come in too).

Could you suggest a more reliable method than “Y close to Y₀” to keep shoes/feet while removing the floor? Is using MEASURE.XYZ as a starting point the right approach?

My goal is a **stable feet-vs-floor split** in a game area, keeping shoes while removing the ground.

Thanks a lot for any best practices or parameters you can share!

Best Regards, Jeff

---

<div class="post-metadata">

**Author:** ![BenjaminV](https://community.stereolabs.com/user_avatar/community.stereolabs.com/benjaminv/32/3863_2.png) [@BenjaminV](https://community.stereolabs.com/u/BenjaminV)\
**Post date:** [September 16, 2025, 8:33am UTC](https://community.stereolabs.com/t/depth-based-humanoid-mask-feet-vs-floor-separation-issues/9879/4 "2025-09-16T08:33:54Z")

</div>

I guess the most important thing is to make sure the camera’s estimated pose is correct, otherwise the plane you will use to remove the floor will not be aligned with the floor, which can create some issues as well.  
It’s also possible that the depth values on your shoes are not correct. Is it possible for you to display the point cloud to validate the depth at your feet ?