# Contradiction in FOV specifications?

**URL:** <https://community.stereolabs.com/t/contradiction-in-fov-specifications/8555>\
**Category:** ZED Mini\
**Created:** [April 8, 2025, 10:12am UTC](https://community.stereolabs.com/t/contradiction-in-fov-specifications/8555 "2025-04-08T10:12:20Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![Nathaniel](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/n/ba8739/32.png) [@Nathaniel](https://community.stereolabs.com/u/Nathaniel)\
**Post date:** [April 8, 2025, 10:12am UTC](https://community.stereolabs.com/t/contradiction-in-fov-specifications/8555/1 "2025-04-08T10:12:20Z")

</div>

Looking at the [specs](https://www.stereolabs.com/en-il/store/products/zed-mini), the field of view for the Zed Mini is listed as 102° x 57°.

However, on [this page](https://support.stereolabs.com/hc/en-us/articles/360007395634-What-is-the-camera-focal-length-and-field-of-view), the widest FOV listed for the Zed Mini is in WVGA mode and is only 85° x 54°! I understand that the rectified image may be somewhat smaller than the lens depending on format, but this is a major reduction in FOV.

For reference, the Zed X Mini shows 110° x 80° in the specification, and 105° x 78° as the maximum FOV in the rectified table, which is much more consistent.

So, For the Zed Mini, which of the numbers is correct?

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [April 8, 2025, 10:29am UTC](https://community.stereolabs.com/t/contradiction-in-fov-specifications/8555/2 "2025-04-08T10:29:49Z")

</div>

> [@Nathaniel](#):
>
> Looking at the [specs](https://www.stereolabs.com/en-il/store/products/zed-mini), the field of view for the Zed Mini is listed as 102° x 57°.

This is correct: Field of Viev 102° (H) x 57° (V) x 118° (D) **max.**  
This is the field of view for RAW not rectified images.

> [@Nathaniel](#):
>
> However, on [this page](https://support.stereolabs.com/hc/en-us/articles/360007395634-What-is-the-camera-focal-length-and-field-of-view), the widest FOV listed for the Zed Mini is in WVGA mode and is only 85° x 54°!

This is correct. This is the field of view of the rectified images.

The ZED Mini mounts “almost” fish-eye lenses with a big distortion, causing a big reduction of the field of view after the rectification.

You can validate these values by running the ZED SDK and [retrieving the field of view values at runtime](https://www.stereolabs.com/docs/api/structsl_1_1CameraParameters.html).