# Cannot set custom object runtime parameters with custom segmentation model?

**URL:** <https://community.stereolabs.com/t/cannot-set-custom-object-runtime-parameters-with-custom-segmentation-model/10682>\
**Category:** C++\
**Tags:** ros2\
**Created:** [January 23, 2026, 10:00pm UTC](https://community.stereolabs.com/t/cannot-set-custom-object-runtime-parameters-with-custom-segmentation-model/10682 "2026-01-23T22:00:25Z")\
**Posts on this page:** 10\
**Page:** 1

<div class="post-metadata">

**Author:** ![17njensen](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/1/58956e/32.png) [@17njensen](https://community.stereolabs.com/u/17njensen)\
**Post date:** [January 23, 2026, 10:00pm UTC](https://community.stereolabs.com/t/cannot-set-custom-object-runtime-parameters-with-custom-segmentation-model/10682/1 "2026-01-23T22:00:26Z")

</div>

I am working on implementing custom YOLO segmentation masking into my ROS2 node and have come across an issue where I cannot call **setCustomObjectDetectionRuntimeParameters** without the process failing. No error is given. If I remove this line and use, I’m assuming, default parameters the process works.

Am I able to set custom object/class parameters if the model is a segmentation model? If I remove this function call, my segmentation detections work but I can’t set properties like is\_static, is\_grounded, tracking\_timeout, etc.

---

<div class="post-metadata">

**Author:** ![mattrouss](https://community.stereolabs.com/user_avatar/community.stereolabs.com/mattrouss/32/2452_2.png) [@mattrouss](https://community.stereolabs.com/u/mattrouss)\
**Post date:** [January 26, 2026, 1:04pm UTC](https://community.stereolabs.com/t/cannot-set-custom-object-runtime-parameters-with-custom-segmentation-model/10682/2 "2026-01-26T13:04:30Z")

</div>

Hi @17njensen,

We will take a look at this to reproduce. Can you confirm whether you are using the official [ZED ROS2 wrapper](https://github.com/stereolabs/zed-ros2-wrapper) or your own C++ node?

If you can share the JSON result of the ZED\_Diagnostic tool, this would help as well.

---

<div class="post-metadata">

**Author:** ![17njensen](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/1/58956e/32.png) [@17njensen](https://community.stereolabs.com/u/17njensen)\
**Post date:** [January 26, 2026, 2:40pm UTC](https://community.stereolabs.com/t/cannot-set-custom-object-runtime-parameters-with-custom-segmentation-model/10682/3 "2026-01-26T14:40:19Z")

</div>

Hi @mattrouss

It is my own C++ node, though it is mostly merging the ROS2 wrapper into my codebase. As for the JSON result, I am using an SVO recording for my testing. I do not have a ZED camera with me at this moment.

---

<div class="post-metadata">

**Author:** ![mattrouss](https://community.stereolabs.com/user_avatar/community.stereolabs.com/mattrouss/32/2452_2.png) [@mattrouss](https://community.stereolabs.com/u/mattrouss)\
**Post date:** [January 26, 2026, 5:23pm UTC](https://community.stereolabs.com/t/cannot-set-custom-object-runtime-parameters-with-custom-segmentation-model/10682/4 "2026-01-26T17:23:52Z")

</div>

Hi @17njensen,

Are you calling the **setCustomObjectDetectionRuntimeParameters** method before enableObjectDetection? The SDK expects it to be called _after_, which may explain why the parameters are not applied.

---

<div class="post-metadata">

**Author:** ![17njensen](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/1/58956e/32.png) [@17njensen](https://community.stereolabs.com/u/17njensen)\
**Post date:** [January 26, 2026, 6:03pm UTC](https://community.stereolabs.com/t/cannot-set-custom-object-runtime-parameters-with-custom-segmentation-model/10682/5 "2026-01-26T18:03:19Z")

</div>

@mattrouss I just checked and I am calling **setCustomObjectDetectionRuntimeParameters** after **enableObjectDetection**.

---

<div class="post-metadata">

**Author:** ![mattrouss](https://community.stereolabs.com/user_avatar/community.stereolabs.com/mattrouss/32/2452_2.png) [@mattrouss](https://community.stereolabs.com/u/mattrouss)\
**Post date:** [January 27, 2026, 9:29am UTC](https://community.stereolabs.com/t/cannot-set-custom-object-runtime-parameters-with-custom-segmentation-model/10682/6 "2026-01-27T09:29:38Z")

</div>

Do you have the same issue with the official custom segmentation sample: [zed-sdk/object detection/custom detector/cpp/tensorrt\_yolov8\_seg\_onnx at master · stereolabs/zed-sdk · GitHub](https://github.com/stereolabs/zed-sdk/tree/master/object%20detection/custom%20detector/cpp/tensorrt_yolov8_seg_onnx) ?

If not, can you send a code snippet that shows if you are handling the parameters differently?

---

<div class="post-metadata">

**Author:** ![17njensen](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/1/58956e/32.png) [@17njensen](https://community.stereolabs.com/u/17njensen)\
**Post date:** [January 27, 2026, 2:53pm UTC](https://community.stereolabs.com/t/cannot-set-custom-object-runtime-parameters-with-custom-segmentation-model/10682/7 "2026-01-27T14:53:49Z")

</div>

@mattrouss I do get the same issue it seems. To clarify, I can run the custom segmentation sample no problem as the code is given. Making adjustments to that code (the github link you sent) to allow me to add CustomObjectDetectionProperties seems to break things (at least the way I am doing it).

I’ve added a code snippet of adjustments I have made to zed-sdk/object detection/custom detector/cpp/tensorrt\_yolov8\_seg\_onnx/src/main.cpp below. This is how I am doing it in my ROS node as well.

```auto
//...    
    // Custom OD
    sl::ObjectDetectionParameters detection_parameters;
    detection_parameters.enable_tracking = true;
    detection_parameters.enable_segmentation = true;
    detection_parameters.detection_model =
              sl::OBJECT_DETECTION_MODEL::CUSTOM_BOX_OBJECTS;
    state = zed.enableObjectDetection(detection_parameters);
    if (state != sl::ERROR_CODE::SUCCESS) {
        std::cerr << "[ERROR] Enabling Object Detection: " << \
          state << std::endl;
        zed.close();
        return EXIT_FAILURE;
    }

// ---> Changes added here

    std::unordered_map<int, sl::CustomObjectDetectionProperties> class_props;

    size_t number_of_classes = 2; // According to my loaded model
    for (int i = 0; i < number_of_classes; i++) {
        sl::CustomObjectDetectionProperties customOdProperties;
        //--------add properties to customOdProperties-----------
        customOdProperties.enabled = true;
        customOdProperties.is_static = true; 
        // ... (define other properties per class)
        //-------------------------------------------------------
        class_props[i] = customOdProperties;
    }

    sl::CustomObjectDetectionRuntimeParameters runtime_params(
        sl::CustomObjectDetectionProperties{}, // default properties
        class_props
    );

    std::cout << "Setting Custom Runtime Parameters..." << std::endl;
    auto error = zed.setCustomObjectDetectionRuntimeParameters(runtime_params);
    std::cout << "Successfully made it past my issue." << std::endl;

// <--- End of changes

    // Get camera configuration
    sl::CameraConfiguration const camera_config {zed.getCameraInformation().camera_configuration};
    sl::Resolution const pc_resolution {std::min(camera_config.resolution.width, 720), std::min(camera_config.resolution.height, 404)};
    sl::CameraConfiguration const camera_info {zed.getCameraInformation(pc_resolution).camera_configuration};

    // Create OpenGL Viewer
    GLViewer viewer;
    viewer.init(argc, argv, camera_info.calibration_parameters.left_cam, true);

// ...

```

Then when building/running it this is the output I get:

> [2026-01-27 07:53:01 UTC][ZED][INFO] Logging level INFO  
> [2026-01-27 07:53:02 UTC][ZED][INFO] [Init] Serial Number: S/N xxxxxxxxx  
> [2026-01-27 07:53:02 UTC][ZED][INFO] [Init] Depth mode: NEURAL  
> Setting Custom Runtime Parameters…  
> Segmentation fault (core dumped)

Thanks

---

<div class="post-metadata">

**Author:** ![mattrouss](https://community.stereolabs.com/user_avatar/community.stereolabs.com/mattrouss/32/2452_2.png) [@mattrouss](https://community.stereolabs.com/u/mattrouss)\
**Post date:** [January 28, 2026, 6:43pm UTC](https://community.stereolabs.com/t/cannot-set-custom-object-runtime-parameters-with-custom-segmentation-model/10682/8 "2026-01-28T18:43:04Z")

</div>

Hi @17njensen,

We have been able to reproduce the issue on our side, and we are currently preparing a fix for the next version of the SDK.

Thank you for reporting this.

---

<div class="post-metadata">

**Author:** ![17njensen](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/1/58956e/32.png) [@17njensen](https://community.stereolabs.com/u/17njensen)\
**Post date:** [February 12, 2026, 6:26pm UTC](https://community.stereolabs.com/t/cannot-set-custom-object-runtime-parameters-with-custom-segmentation-model/10682/9 "2026-02-12T18:26:10Z")

</div>

@mattrouss Was this added to the latest release? I saw that was posted today (also this latest release sounds amazing!)

---

<div class="post-metadata">

**Author:** ![mattrouss](https://community.stereolabs.com/user_avatar/community.stereolabs.com/mattrouss/32/2452_2.png) [@mattrouss](https://community.stereolabs.com/u/mattrouss)\
**Post date:** [February 13, 2026, 10:22am UTC](https://community.stereolabs.com/t/cannot-set-custom-object-runtime-parameters-with-custom-segmentation-model/10682/10 "2026-02-13T10:22:16Z")

</div>

Hi @17njensen,

The issue was raised a bit short for release 5.2, a fix is currently in review for the next patch release. Sorry for the wait.