# Cameras Sync Options with External Device

**URL:** <https://community.stereolabs.com/t/cameras-sync-options-with-external-device/10561>\
**Category:** ZED X\
**Created:** [December 29, 2025, 11:27am UTC](https://community.stereolabs.com/t/cameras-sync-options-with-external-device/10561 "2025-12-29T11:27:01Z")\
**Posts on this page:** 7\
**Page:** 1

<div class="post-metadata">

**Author:** ![Moh](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/m/b3f665/32.png) [@Moh](https://community.stereolabs.com/u/Moh)\
**Post date:** [December 29, 2025, 11:27am UTC](https://community.stereolabs.com/t/cameras-sync-options-with-external-device/10561/1 "2025-12-29T11:27:02Z")

</div>

Hello,

I’m interested in recording indoor sessions via 2+ cameras that can be **synced** to our Xsens MVN Awinda IMU (inertial measurement units) system. The Xsens base station **has built-in IN/OUT bnc ports** that can be configured to receive or send trigger signals from/to external devices (i.e., it can be configured to Master or Slave).

I think **ZED X cameras** have **sync/trigger capabilities**. Can you please confirm this? Does it still need the **ZED Box Mini** and **ZED Link Capture Card Duo** to perform such sync?

Thanks for your advice.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [December 29, 2025, 11:36am UTC](https://community.stereolabs.com/t/cameras-sync-options-with-external-device/10561/2 "2025-12-29T11:36:42Z")

</div>

Hi @Moh  
Welcome to the [Stereolabs](https://www.stereolabs.com/) community.

This capability is available only when using the [ZED Link Mono](https://www.stereolabs.com/docs/embedded/zed-link/zed-link-mono-triggering), the [ZED Link Quad](https://www.stereolabs.com/docs/embedded/zed-link/zed-link-quad-triggering), or the [ZED Box Mini](https://www.stereolabs.com/docs/embedded/zed-box-mini/connectivity#sync-out).

New documentation with all the details will be released in a few days.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [January 12, 2026, 9:04am UTC](https://community.stereolabs.com/t/cameras-sync-options-with-external-device/10561/3 "2026-01-12T09:04:53Z")

</div>

**Update** the documentation “Hardware triggering” documentation of the [ZED Link Mono](https://www.stereolabs.com/docs/embedded/zed-link/zed-link-mono-triggering), the [ZED Link Quad](https://www.stereolabs.com/docs/embedded/zed-link/zed-link-quad-triggering), and the [ZED Box Mini/Mini Carrier Board](https://www.stereolabs.com/docs/embedded/zed-box-mini/connectivity#sync-out) have been updated to add information about the **SLAVE MODE** and Multi-device synchronization:

> **[ZED Link Mono GPIO Triggering - Stereolabs](https://www.stereolabs.com/docs/embedded/zed-link/zed-link-mono-triggering)**
>
> The ZED Link Mono GMSL2 capture card allows you to synchronize external sensors by using triggering signals on the 6-pin 2mm pitch GPIO connector J4.

> **[ZED Link Quad GPIO Triggering - Stereolabs](https://www.stereolabs.com/docs/embedded/zed-link/zed-link-quad-triggering)**
>
> The ZED Link Quad GMSL2 capture card allows you to synchronize external sensors by using triggering signals on the 16-pin 2mm pitch GPIO connector J17.

> **[ZED Box Mini Connectivity - Stereolabs](https://www.stereolabs.com/docs/embedded/zed-box-mini/connectivity)**
>
> Connection Ports # Front side # Power connector Ethernet connector Power LED indicator Reset button Force Recovery button Left side # \[optional\] Wi-Fi antenna connectors Rear side # USB OTG port USB 3 …

---

<div class="post-metadata">

**Author:** ![Petar](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/dfb087/32.png) [@Petar](https://community.stereolabs.com/u/Petar)\
**Post date:** [February 9, 2026, 11:37am UTC](https://community.stereolabs.com/t/cameras-sync-options-with-external-device/10561/4 "2026-02-09T11:37:27Z")

</div>

Hi @Myzhar ,

I am working with **ZED link DUO** card and two cameras. As you mentioned only Mono, Quad and Mini, support HW GPIO trigger in SLAVE mode. Any chance this will be implemented with **Duo card** or the card will never support GPIO triggering?

Thanks, Petar

---

<div class="post-metadata">

**Author:** ![Parv-Maheshwari](https://community.stereolabs.com/user_avatar/community.stereolabs.com/parv-maheshwari/32/5756_2.png) [@Parv-Maheshwari](https://community.stereolabs.com/u/Parv-Maheshwari)\
**Post date:** [February 9, 2026, 8:20pm UTC](https://community.stereolabs.com/t/cameras-sync-options-with-external-device/10561/5 "2026-02-09T20:20:45Z")

</div>

Hi @Myzhar Regarding slave mode on the quad capture card - how is the camera capture time, exposure start/end time and the image timestamps related to the input trigger.

With the master mode it is clearly documented that the `The output trigger signals are two square waves, with their rising edges synchronized with the end of the exposure phase of the CMOS sensors.`

---

<div class="post-metadata">

**Author:** ![cd\_0811](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/c/97f17d/32.png) [@cd\_0811](https://community.stereolabs.com/u/cd_0811)\
**Post date:** [February 11, 2026, 8:23am UTC](https://community.stereolabs.com/t/cameras-sync-options-with-external-device/10561/6 "2026-02-11T08:23:47Z")

</div>

Hi @Myzhar ，

I’m a bit confused about whether this capture card [ZED Link Duo on Xavier AGX](https://www.stereolabs.com/docs/embedded/zed-link/dual-jetson-xavier-agx-devkit-setup) supports external triggering, or if I need to use a different card to trigger the camera externally。

Thanks.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [February 11, 2026, 8:25am UTC](https://community.stereolabs.com/t/cameras-sync-options-with-external-device/10561/7 "2026-02-11T08:25:59Z")

</div>

> [@cd\_0811](#):
>
> I’m a bit confused about whether this capture card [ZED Link Duo on Xavier AGX](https://www.stereolabs.com/docs/embedded/zed-link/dual-jetson-xavier-agx-devkit-setup) supports external triggering

The ZED Link Duo does not support external triggering.  
Only the ZED Link Mono and the ZED Link Quad provide this behavior.