# Cameras do not stream video

**URL:** <https://community.stereolabs.com/t/cameras-do-not-stream-video/11772>\
**Category:** Software\
**Tags:** sdk, zed-sdk, ros, jetson\
**Created:** [October 7, 2026, 11:34am UTC](https://community.stereolabs.com/t/cameras-do-not-stream-video/11772 "2026-10-07T11:34:21Z")\
**Posts on this page:** 9\
**Page:** 1

<div class="post-metadata">

**Author:** ![SirMichcik](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/s/b5a626/32.png) [@SirMichcik](https://community.stereolabs.com/u/SirMichcik)\
**Post date:** [October 7, 2026, 11:34am UTC](https://community.stereolabs.com/t/cameras-do-not-stream-video/11772/1 "2026-10-07T11:34:21Z")

</div>

Hi,

I’m having trouble getting two [Stereolabs](https://www.stereolabs.com/) ZED XOne GS cameras working on a Jetson.

System:

- Jetson Orin

- JetPack 6.2.1

- L4T 36.4.4

- Linux kernel 5.15.148

- CUDA 12.6

- TensorRT 10.3.0

- cuDNN 9.3.0.75

Cameras / ZED:

- 2 × ZED XOne GS

- GMSL via MAX96712

- ZED SDK 5.5.0

- ZEDLink Duo 1.4.3-LI-MAX96712-L4T36.4.0

The cameras are correctly detected by ZED Explorer, GMSL/I2C communication works, the kernel detects both sensors, and `/dev/video0` and `/dev/video1` are created.

However, the cameras cannot actually stream any frames. Even using `v4l2-ctl` directly on the host, no frames are received.

The ZED SDK then fails with:

`CAMERA FAILED TO SETUP`

and the process exits with code `-11`.

Im trying to launch them with ros2 wrapper in docker and it returns with a log:

`component_container_isolated-1] [2026-10-06 18:33:24 UTC][ZED][ERROR] [ZED-Argus][Critical] Cannot create iQueue (produceSingleV5)`

I have already:

- upgraded ZED SDK from 5.2.2 to 5.5.0,

- reinstalled the `stereolabs-zedlink-duo` package,

- verified that the cameras are detected correctly,

- tested the cameras directly through V4L2.

The problem seems to be somewhere between the ZED sensor/GMSL pipeline and the Jetson VI/CSI capture layer.

Has anyone successfully run ZED XOne GS + ZEDLink Duo MAX96712 on JetPack 6.2.1 / L4T 36.4.4? Thanks!

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [October 7, 2026, 2:26pm UTC](https://community.stereolabs.com/t/cameras-do-not-stream-video/11772/2 "2026-10-07T14:26:11Z")

</div>

Hi @SirMichcik  
Welcome to the [StereoLabs](https://www.stereolabs.com/) community.

> [@SirMichcik](#):
>
> - Jetson Orin

This is a generic information. What type of Jetson Orin are you using?

> [@SirMichcik](#):
>
> The ZED SDK then fails with:
> 
> `CAMERA FAILED TO SETUP`
> 
> and the process exits with code `-11`.

Please share the code that you are using.

---

<div class="post-metadata">

**Author:** ![SirMichcik](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/s/b5a626/32.png) [@SirMichcik](https://community.stereolabs.com/u/SirMichcik)\
**Post date:** [October 8, 2026, 7:29am UTC](https://community.stereolabs.com/t/cameras-do-not-stream-video/11772/3 "2026-10-08T07:29:31Z")

</div>

Thanks for the reply.

> [@Myzhar](#):
>
> This is a generic information. What type of Jetson Orin are you using?

I am using NVIDIA Jetson Orin NX Engineering Reference Developer Kit

> [@Myzhar](#):
>
> Please share the code that you are using.

Im launching `ros2 launch zed_wrapper zed_camera.launch.py camera_model:=zedxonegs camera_name:=zed_front` on the 5.5.0 zed\_ros2\_wrapper pkg.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [October 8, 2026, 9:13am UTC](https://community.stereolabs.com/t/cameras-do-not-stream-video/11772/4 "2026-10-08T09:13:51Z")

</div>

> [@SirMichcik](#):
>
> I am using NVIDIA Jetson Orin NX Engineering Reference Developer Kit

Who is the producer? This is not a device supported by the ZED X Driver.  
You need a custom driver to use this board with our cameras.

You have two options:

- contact the producer and ask to them to develop a custom driver
- contact us at [support@stereolabs.com](mailto:support@stereolabs.com) to ask to be invited to the GitHub repository of the ZED X Driver to develop a compatible driver yourself

---

<div class="post-metadata">

**Author:** ![SirMichcik](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/s/b5a626/32.png) [@SirMichcik](https://community.stereolabs.com/u/SirMichcik)\
**Post date:** [October 8, 2026, 1:11pm UTC](https://community.stereolabs.com/t/cameras-do-not-stream-video/11772/5 "2026-10-08T13:11:18Z")

</div>

I understand that it may not be directly supported, although it was working on 5.2.2 before. Perfectly fine with 1 camera, problems with stability occured after adding 2nd camera and then upgrading to 5.5 results in errors above. Therefore i am quite certain that correct setup is possible on this hardware configuration.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [October 8, 2026, 1:15pm UTC](https://community.stereolabs.com/t/cameras-do-not-stream-video/11772/6 "2026-10-08T13:15:39Z")

</div>

> [@SirMichcik](#):
>
> Therefore i am quite certain that correct setup is possible on this hardware configuration.

Unfortunately, we cannot support you with this because this is not an officially supported configuration.

---

<div class="post-metadata">

**Author:** ![SirMichcik](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/s/b5a626/32.png) [@SirMichcik](https://community.stereolabs.com/u/SirMichcik)\
**Post date:** [October 8, 2026, 2:15pm UTC](https://community.stereolabs.com/t/cameras-do-not-stream-video/11772/7 "2026-10-08T14:15:32Z")

</div>

Could you at least point me in the right direction with `component_container_isolated-1] [2026-10-06 18:33:24 UTC][ZED][ERROR] [ZED-Argus][Critical] Cannot create iQueue (produceSingleV5) `error?

Also, i have just tested that camera is streaming with ZED\_Explorer when the graphical interface is active.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [October 8, 2026, 4:45pm UTC](https://community.stereolabs.com/t/cameras-do-not-stream-video/11772/8 "2026-10-08T16:45:59Z")

</div>

> [@SirMichcik](#):
>
> Also, i have just tested that camera is streaming with ZED\_Explorer when the graphical interface is active.

Do you mean that with ZED Explorer and a connected screen it works as expected?  
Is it the same with ZED Depth Viewer?

---

<div class="post-metadata">

**Author:** ![SirMichcik](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/s/b5a626/32.png) [@SirMichcik](https://community.stereolabs.com/u/SirMichcik)\
**Post date:** [October 12, 2026, 11:27am UTC](https://community.stereolabs.com/t/cameras-do-not-stream-video/11772/9 "2026-10-12T11:27:29Z")

</div>

> [@Myzhar](#):
>
> Do you mean that with ZED Explorer and a connected screen it works as expected?

Exactly, after connecting a display i can see camera stream on ZED\_Explorer.

> [@Myzhar](#):
>
> Is it the same with ZED Depth Viewer?

No, here i get “waiting for camera” while ZED\_Explorer is streaming the video at the same time.