# Camera Hardware Failure During Streaming (Requires Unplug)

**URL:** <https://community.stereolabs.com/t/camera-hardware-failure-during-streaming-requires-unplug/3590>\
**Category:** Python\
**Created:** [September 27, 2023, 7:56pm UTC](https://community.stereolabs.com/t/camera-hardware-failure-during-streaming-requires-unplug/3590 "2023-09-27T19:56:03Z")\
**Posts on this page:** 4\
**Page:** 1

<div class="post-metadata">

**Author:** ![pproctor](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/5e9695/32.png) [@pproctor](https://community.stereolabs.com/u/pproctor)\
**Post date:** [September 27, 2023, 7:56pm UTC](https://community.stereolabs.com/t/camera-hardware-failure-during-streaming-requires-unplug/3590/1 "2023-09-27T19:56:03Z")

</div>

I’m running the Camera Streaming Sender example, and over the course of a few hours running 4 cameras and fusion, I have seen multiple camera hardware crashes on the sender with this message:

```auto

.......................[ZED][ERROR] [Grab] Failed to recover image capture... Timeout.
[ZED][WARNING] CAMERA NOT DETECTED in sl::ERROR_CODE sl::Camera::grab(sl::RuntimeParameters)
[ZED][Grab] Detected Connection Failure. Trying to recover the camera with sn 37415635 ...
..[ZED][INFO] [Grab] Camera module reset

```

The fusion server eventually times out with the message:  
`packet queue is empty, aborting`

Trying to restart the sender does not work, and gives the message:

```auto
[Sample] Using default resolution
[ZED][INFO] Logging level INFO
[ZED][WARNING] CAMERA NOT DETECTED in sl::ERROR_CODE sl::Camera::open(sl::InitParameters)
Camera Open : CAMERA NOT DETECTED. Exit program.
[ZED][ERROR] [ZED] sl::Camera::Open has not been called, no Camera instance running.

```

The only solution that has worked thus far is unplugging and replugging the USB for the camera. This has happened on two cameras, so I don’t think this is an issue of a bad camera, or hardware failure. Would love to hear any suggestions.

---

<div class="post-metadata">

**Author:** ![BenjaminV](https://community.stereolabs.com/user_avatar/community.stereolabs.com/benjaminv/32/3863_2.png) [@BenjaminV](https://community.stereolabs.com/u/BenjaminV)\
**Post date:** [September 29, 2023, 10:01am UTC](https://community.stereolabs.com/t/camera-hardware-failure-during-streaming-requires-unplug/3590/3 "2023-09-29T10:01:05Z")

</div>

Thanks for the feedback, I’ll share it with the team so they can investigate this.

What power mode are you using on your jetson using POE?

Stereolabs Support

---

<div class="post-metadata">

**Author:** ![pproctor](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/5e9695/32.png) [@pproctor](https://community.stereolabs.com/u/pproctor)\
**Post date:** [October 4, 2023, 5:33pm UTC](https://community.stereolabs.com/t/camera-hardware-failure-during-streaming-requires-unplug/3590/4 "2023-10-04T17:33:29Z")

</div>

I believe it was 6 cores 15W.

---

<div class="post-metadata">

**Author:** ![Jay.richards](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/j/ed8c4c/32.png) [@Jay.richards](https://community.stereolabs.com/u/Jay.richards)\
**Post date:** [November 2, 2023, 11:37pm UTC](https://community.stereolabs.com/t/camera-hardware-failure-during-streaming-requires-unplug/3590/5 "2023-11-02T23:37:38Z")

</div>

Did this get resolved? we have the same issue.