# Body Tracking with UE5: Possible errors in tutorial?

**URL:** <https://community.stereolabs.com/t/body-tracking-with-ue5-possible-errors-in-tutorial/10014>\
**Category:** Unreal Engine\
**Created:** [September 26, 2025, 1:46pm UTC](https://community.stereolabs.com/t/body-tracking-with-ue5-possible-errors-in-tutorial/10014 "2025-09-26T13:46:16Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![ygreq](https://community.stereolabs.com/user_avatar/community.stereolabs.com/ygreq/32/5041_2.png) [@ygreq](https://community.stereolabs.com/u/ygreq)\
**Post date:** [September 26, 2025, 1:46pm UTC](https://community.stereolabs.com/t/body-tracking-with-ue5-possible-errors-in-tutorial/10014/1 "2025-09-26T13:46:16Z")

</div>

Hi folks!

I see mismatched information presented in the [Body Tracking with UE5](https://www.stereolabs.com/docs/ue5/body-tracking)tutorial in regards to last steps. And I want to be sure if I understand correctly.

At the **[Create an actor](https://www.stereolabs.com/docs/ue5/body-tracking#create-an-actor)** step, it says the following: Create a child actor to `BP_ZED_Manny`

But then at [Use the actor with the visualizer](https://www.stereolabs.com/docs/ue5/body-tracking#use-the-actor-with-the-visualizer) step, it says to “Replace the `BP_ZED_Manny` actor with your new one in the `BP_BodyTracking_Visualizer"`

Nowhere does it say that you should create a backup of the `BP\_ZED\_Manny’ asset and call it something like BP\_ZED\_Manny\_v2 or something like that and than attribute that to the BP\_BodyTracking\_Visualizer. Right?

Also I see that there is no option for “Avatars Visible” like presented in the tutorial. Does “Use Retargeter” have the same function?

Thank you so much for clarifying this and if I am right, maybe correcting the tutorial to be more meaningful.

---

<div class="post-metadata">

**Author:** ![ygreq](https://community.stereolabs.com/user_avatar/community.stereolabs.com/ygreq/32/5041_2.png) [@ygreq](https://community.stereolabs.com/u/ygreq)\
**Post date:** [September 26, 2025, 2:03pm UTC](https://community.stereolabs.com/t/body-tracking-with-ue5-possible-errors-in-tutorial/10014/2 "2025-09-26T14:03:24Z")

</div>

Regarding this [quote=“ygreq, post:1, topic:10014”]  
Nowhere does it say that you should create a backup of the `BP\_ZED\_Manny’ asset and call it something like BP\_ZED\_Manny\_v2 or something like that and than attribute that to the BP\_BodyTracking\_Visualizer. Right?  
[/quote]

I see that if you make a duplicate of the BP\_ZED\_Manny and then use that instead of the original in the BP\_BodyTracking\_Visualize, UE crashes. If I put back the initial BP\_ZED\_Manny, everything works fine. Is this normal?