# Body tracking with a camera in portrait mode: status after SDK 5.5 and GEN\_2

**URL:** <https://community.stereolabs.com/t/body-tracking-with-a-camera-in-portrait-mode-status-after-sdk-5-5-and-gen-2/11774>\
**Category:** Software\
**Tags:** sdk\
**Created:** [October 7, 2026, 11:34am UTC](https://community.stereolabs.com/t/body-tracking-with-a-camera-in-portrait-mode-status-after-sdk-5-5-and-gen-2/11774 "2026-10-07T11:34:43Z")\
**Posts on this page:** 5\
**Page:** 1

<div class="post-metadata">

**Author:** ![PointCloudNine](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/c2a13f/32.png) [@PointCloudNine](https://community.stereolabs.com/u/PointCloudNine)\
**Post date:** [October 7, 2026, 11:34am UTC](https://community.stereolabs.com/t/body-tracking-with-a-camera-in-portrait-mode-status-after-sdk-5-5-and-gen-2/11774/1 "2026-10-07T11:34:43Z")

</div>

Hi [Stereolabs](https://www.stereolabs.com/) team and community,

We would like to pick up a topic that has come up in several threads over the past years: body tracking with a ZED camera mounted in portrait orientation (rolled by 90°). We tested the new GEN\_2 model in SDK 5.5 (without the impression that it’s solved after comparing both, landscape and portrait orientation tracking) and would like to know where this topic stands and how you recommend we deal with it.

We have several questions down the same avenue:

1. Do we miss something that enables body tracking with a camera in portrait mode? Does GEN\_2 address camera roll, or only body orientation relative to an upright camera?
2. Does the body tracking module use the IMU or gravity to compensate for any camera orientation?
3. Without the IMU, is there a supported way to give the SDK the fixed camera orientation (for example initial\_world\_transform in PositionalTrackingParameters) which also has an effect on the body tracking itself?
4. If none of the above points holds true, what do you recommend? For example, can we rotate the images before they reach the body tracking module?
5. And most importantly is camera roll support for body tracking on your roadmap, and if so, for which release?

We can also share short SVO2 recordings of both orientations via pm.

/PointCloudNine

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [October 7, 2026, 3:31pm UTC](https://community.stereolabs.com/t/body-tracking-with-a-camera-in-portrait-mode-status-after-sdk-5-5-and-gen-2/11774/2 "2026-10-07T15:31:28Z")

</div>

Hi @PointCloudNine,  
Welcome to the [StereoLabs](https://www.stereolabs.com/) community.

I’ve forwarded all the details that you reported here to the ZED SDK team to try to replicate the behavior in our labs and understand if it’s expected.

> [@PointCloudNine](#):
>
> We can also share short SVO2 recordings of both orientations via pm.

This would be greate. Please share them via email to [support@stereolabs.com](mailto:support@stereolabs.com)

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [October 8, 2026, 1:13pm UTC](https://community.stereolabs.com/t/body-tracking-with-a-camera-in-portrait-mode-status-after-sdk-5-5-and-gen-2/11774/3 "2026-10-08T13:13:55Z")

</div>

@PointCloudNine can you please confirm that you tested Body Tracking GEN\_2 with the Body Tracking **ACCURATE** model?

If you do not use the ACCURATE model, the SDK safely falls back to GEN\_1.

Can you please share a code snippet with the configuration parameters that you used?

---

<div class="post-metadata">

**Author:** ![PointCloudNine](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/p/c2a13f/32.png) [@PointCloudNine](https://community.stereolabs.com/u/PointCloudNine)\
**Post date:** [October 15, 2026, 8:44am UTC](https://community.stereolabs.com/t/body-tracking-with-a-camera-in-portrait-mode-status-after-sdk-5-5-and-gen-2/11774/4 "2026-10-15T08:44:43Z")

</div>

Hi @Myzhar,

> can you please confirm that you tested Body Tracking GEN\_2 with the Body Tracking **ACCURATE** model?

Hereby confirmed.

> Can you please share a code snippet with the configuration parameters that you used?

Our setup is a ZED X with SDK 5.5.0. The camera is fixed and rolled by 90°.

Parameters:

```auto
sl::PositionalTrackingParameters pt;
pt.set_as_static = true; // no initial_world_transform

sl::BodyTrackingParameters bt;
bt.detection_model = sl::BODY_TRACKING_MODEL::HUMAN_BODY_ACCURATE;
bt.body_format = sl::BODY_FORMAT::BODY_34;
bt.model_gen = sl::BODY_TRACKING_MODEL_GEN::GEN_2;
bt.enable_body_fitting = true;

```

Camera opened at HD1080, 30 fps, `DEPTH_MODE::NEURAL_LIGHT`. Runtime `detection_confidence_threshold = 40`. All other parameters are SDK defaults.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [October 16, 2026, 9:00am UTC](https://community.stereolabs.com/t/body-tracking-with-a-camera-in-portrait-mode-status-after-sdk-5-5-and-gen-2/11774/5 "2026-10-16T09:00:26Z")

</div>

Hi @PointCloudNine  
Thank you for the details.

The SDK Team noted this problem and will work on a fix as soon as possible.  
I will send you an update as soon as I get some news.