# Accuracy of positional tracking

**URL:** <https://community.stereolabs.com/t/accuracy-of-positional-tracking/9174>\
**Category:** ZED Mini\
**Tags:** python, sdk\
**Created:** [June 26, 2025, 8:36am UTC](https://community.stereolabs.com/t/accuracy-of-positional-tracking/9174 "2025-06-26T08:36:12Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![mpiseno](https://community.stereolabs.com/user_avatar/community.stereolabs.com/mpiseno/32/4567_2.png) [@mpiseno](https://community.stereolabs.com/u/mpiseno)\
**Post date:** [June 26, 2025, 8:36am UTC](https://community.stereolabs.com/t/accuracy-of-positional-tracking/9174/1 "2025-06-26T08:36:12Z")

</div>

I am using the PositionalTracking module to get the camera pose in the world frame following a script similar to example code [tutorial](https://github.com/stereolabs/zed-sdk/blob/master/positional%20tracking/positional%20tracking/python/positional_tracking.py). I am having an issue with the translation accuracy, which seems to drift quickly and can have very large errors (sometimes around 30cm). I am just running the program, lifting the camera up and down a few times (with smooth movements), and setting it back down on the table so that the height should return to 0.

## System Information

Camera: Zed Mini  
SDK Version: 5.0.2  
OS: Ubuntu 24  
Python version: 3.10

## Code

```auto
import sys
import time
import numpy as np
import pyzed.sl as sl

zed = sl.Camera()

init_params = sl.InitParameters()
init_params.camera_resolution = sl.RESOLUTION.HD720
init_params.camera_fps = 30
init_params.coordinate_system = sl.COORDINATE_SYSTEM.RIGHT_HANDED_Y_UP
init_params.coordinate_units = sl.UNIT.METER
zed.open(init_params)

tracking_params = sl.PositionalTrackingParameters()
tracking_params.enable_imu_fusion = True
tracking_params.mode = sl.POSITIONAL_TRACKING_MODE.GEN_1
status = zed.enable_positional_tracking(tracking_params) #enable Positional Tracking
if status != sl.ERROR_CODE.SUCCESS:
    print("[Sample] Enable Positional Tracking : "+repr(status)+". Exit program.")
    zed.close()
    sys.exit()

runtime_parameters = sl.RuntimeParameters()
zed_pose = sl.Pose()
translation = sl.Translation()
orientation = sl.Orientation()
try:
    while True:
        if zed.grab(runtime_parameters) == sl.ERROR_CODE.SUCCESS:
            # Get the pose of the camera relative to the world frame
            state = zed.get_position(zed_pose, sl.REFERENCE_FRAME.WORLD)
            Tx = np.round(zed_pose.get_translation(translation).get()[:3], 3)
            print(f"Translation: {Tx}, timestamp: {zed_pose.timestamp.get_seconds()}")

        time.sleep(0.001)
finally:
    zed.close()

```

## Output

I am looking at the value of the Y axis, which is the height. It should return back to 0 since I lift the camera up starting on a tabletop and then place it down on the same table. As you can see below there is 17cm of error. In other repetitions of this experiment I sometimes see even larger error.

```auto
Translation: [0.0, 0.0, 0.0]
...
...
...
Translation: [-0.13 -0.174 -0.028]

```

**Other Information:** I tested with GEN\_2 and GEN\_3 as well. GEN\_3 seems to provide much more accurate results in the same experiment (less than 1cm error). GEN\_2 still has a lot of error.

**Question:** Is this level of accuracy expected or am I doing something wrong? Is there anything else I can do to improve the accuracy besides what is shown in my code?

---

<div class="post-metadata">

**Author:** ![TanguyHardelin](https://community.stereolabs.com/user_avatar/community.stereolabs.com/tanguyhardelin/32/1298_2.png) [@TanguyHardelin](https://community.stereolabs.com/u/TanguyHardelin)\
**Post date:** [June 27, 2025, 8:40am UTC](https://community.stereolabs.com/t/accuracy-of-positional-tracking/9174/2 "2025-06-27T08:40:02Z")

</div>

Hello @mpiseno,  
Thanks for your feedback !

> [@mpiseno](#):
>
> **Other Information:** I tested with GEN\_2 and GEN\_3 as well. GEN\_3 seems to provide much more accurate results in the same experiment (less than 1cm error). GEN\_2 still has a lot of error.

Indeed `GEN_1` and `GEN_2` are old tracking mode, prefer to use`GEN_3` in your experiment. `GEN_3` will be our reference SLAM algorithm for next release.

> [@mpiseno](#):
>
> **Question:** Is this level of accuracy expected or am I doing something wrong? Is there anything else I can do to improve the accuracy besides what is shown in my code?

The expected level of accuracy for `GEN_3` is below 1% drift. However, depending on your environment, movement, and vibration, this accuracy could be degraded.

That said, I can give you a few tips:

- If you use `GEN_3` , consider disabling depth computation. This should improve your runtime and tracking accuracy. Indeed, the fewer frames the tracking drops, the more accurate it is.
- For both tracking versions, ensure smooth movement and avoid camera vibration. Since `GEN_3` uses IMU information, vibration on the camera can particularly degrade accuracy. This also applies to IMU saturation.

I hope this answers your question.

Best regards,  
Tanguy