Hi
I compiled this example with cmake, opened the .sln file with vs2022, and finally showed that there was no GPU compatible, and I used version zedSDK_3.7.4, cuda_11.5,
Can you teach me how to solve it?
Hello, and thank you for reaching out.
What GPU and nvidia driver do you have ? Can you send us the output of the application “ZED Diagnostics”, which we provide with the SDK?
Best regards
Antoine Lassagne
Senior Developer - ZED SDK
Stereolabs Support
hi
maybe these are the output logs
CL.command.1.tlog (3.5 KB)
CL.read.1.tlog (92.1 KB)
CL.write.1.tlog (2.1 KB)
CustomBuild.command.1.tlog (595 Bytes)
CustomBuild.read.1.tlog (2.7 KB)
CustomBuild.write.1.tlog (194 Bytes)
link.command.1.tlog (4.1 KB)
link.read.1.tlog (5.4 KB)
link.write.1.tlog (1.2 KB)
ZED_Point_Cloud_Mapping.lastbuildstate (207 Bytes)ZED_Point_Cloud_Mapping.log (6.9 KB)
Hi
and these are the output logs
CL.command.1.tlog (3.5 KB)
CL.read.1.tlog (92.1 KB)
CL.write.1.tlog (2.1 KB)
CustomBuild.command.1.tlog (595 Bytes)
CustomBuild.read.1.tlog (2.7 KB)
CustomBuild.write.1.tlog (194 Bytes)
link.command.1.tlog (4.1 KB)
link.read.1.tlog (5.4 KB)
link.write.1.tlog (1.2 KB)
ZED_Point_Cloud_Mapping.lastbuildstate (207 Bytes)ZED_Point_Cloud_Mapping.log (6.9 KB)
Hello, and thank you for reaching out.
Best wishes
Hello
This problem has been resolved, the error is a high version of the cuda path left in the computer system variable