After following the installation instructions for ZED 3.7 SDK for Jetpack 4.6 (L4T 32.6) on a Jetson Nano with Cuda 10.2 the tool ZED_Depth_Viewer produces the following error after opening the application and then immediately closing:
Stack trace (most recent call last):
#0 Object "/usr/lib/aarch64-linux-gnu/libQt5OpenGL.so.5", at 0x7fa3506ad0, in QGLContext::contextHandle() const
Segmentation fault (Address not mapped to object [0x8])
Segmentation fault (core dumped)
OpenGL was installed using these instructions.
pyopengl has been installed, along with the other python dependencies, and the default python is 3.6.9
Was something overlooked in the installation causing the Depth Viewer to fail?