my first time to run the tools/ZED_Depth_Viewer on Ubuntu18.04, cuda10.2, zed sdk version is 3.7.6
In addition, the ZED_Explorer works normally
has anybody know how to solve it?
ubuntu@ubu:/usr/local/zed/tools$ ./ZED_Depth_Viewer
Stack trace (most recent call last):
#6 Object "[0xffffffffffffffff]", at 0xffffffffffffffff, in
#5 Object "./ZED_Depth_Viewer", at 0x420259, in
#4 Object "/lib/x86_64-linux-gnu/libc.so.6", at 0x7ff24c895bf6, in __libc_start_main
#3 Object "./ZED_Depth_Viewer", at 0x41da00, in
#2 Object "./ZED_Depth_Viewer", at 0x43d07a, in
#1 Object "/usr/local/zed/lib/libsl_zed.so", at 0x7ff24fcd27a9, in sl::Camera::checkAIModelStatus(sl::AI_MODELS, int)
#0 Object "/usr/local/zed/lib/libsl_zed.so", at 0x7ff24fade7fe, in
Speicherzugriffsfehler (Adresse ist nicht mit dem Objekt verbunden [(nil)])
Speicherzugriffsfehler (Speicherabzug geschrieben)
also the same problem when it runs to the AI Models
ubuntu@ubu:/usr/local/zed/tools$ ./ZED_Diagnostic
QNetworkReplyHttpImplPrivate::_q_startOperation was called more than once QUrl("http://download.stereolabs.com/.zedsdk_update.json")
Incompatible CUDNN version (found 8.100000, minimum required 8.204000)
libpng warning: iCCP: known incorrect sRGB profile
libpng warning: iCCP: known incorrect sRGB profile
libpng warning: iCCP: known incorrect sRGB profile
Stack trace (most recent call last) in thread 5789:
#6 Object "[0xffffffffffffffff]", at 0xffffffffffffffff, in
#5 Object "/lib/x86_64-linux-gnu/libc.so.6", at 0x7f881b96971e, in clone
#4 Object "/lib/x86_64-linux-gnu/libpthread.so.0", at 0x7f881d4776da, in
#3 Object "/usr/lib/x86_64-linux-gnu/libstdc++.so.6", at 0x7f881c2ac6de, in
#2 Object "./ZED_Diagnostic", at 0x43b603, in
#1 Object "./ZED_Diagnostic", at 0x4640fc, in
#0 Object "./ZED_Diagnostic", at 0x4733e2, in
Speicherzugriffsfehler (Adresse ist nicht mit dem Objekt verbunden [(nil)])
Speicherzugriffsfehler (Speicherabzug geschrieben)
ubuntu@ubu:/usr/local/zed/tools$ ./ZED_Diagnostic -c
ZED Diagnostic Tool
QNetworkReplyHttpImplPrivate::_q_startOperation was called more than once QUrl("http://download.stereolabs.com/.zedsdk_update.json")
Incompatible CUDNN version (found 8.100000, minimum required 8.204000)
- Running ZED SDK Diagnostic : Warning
Object detection module corrupted. Please reinstall the ZED SDK and enable the Object Detection option.
ZED SDK version: 3.7.6
CUDA version: V10.2.89
- Running Processor Diagnostic : Warning
Unable to identify your processor, make sure that it fits the requirements.
Motherboard: B365 M AORUS ELITE-CF, Gigabyte Technology Co., Ltd.
- Running Graphics Card Diagnostic : OK
Graphics card: GeForce RTX 2080 Ti
- Running Camera Test Diagnostic : OK
Camera: ZED 2
Firmware: 1523
- Running USB Diagnostic : OK
USB Bandwidth: OK
Diagnostic finished, a file has been generated : ZED_Diagnostic_Results.json
The problem with your configuration is that you are using CUDA 10.2 with an RTX GPU card.
I suggest you uninstall CUDA, download the ZED SDK v3.7.7 for CUDA 11.7, and let the installer guide you to install the required CUDA version.