Hi,
No problems with the tutorials but I can’t run the examples like body tracking, object detection and positional tracking.
My sys:
Windows 10(x64)
Cuda 11
Python 3.10.7
#NullFuctionError
Attempt to call an undifined function gluInit, ckeck for bool(gluInit) before calling
File “C:\Program Files (x86) \ZED SDK\samples\bodytracking\python\ogl_viewer\viewer.py”,line819,ininitglutinitO
File “C: \Program Files (×86)\ZED SDK\samples\bodytracking\python\body_tracking.py”, line 86, in viewer.init(camera_info.calibration_parameters.left_cam,
obj_param.enable_tracking,obj_param.body_format)
when I try to initialize by changing parameters or something and tells me that it can’t find:
from cv_viewer.utils import *
Does anyone have any advice?