Missing sl_ai library

I’ve installed the latest SDK 3.7.6 multiple times. sl_ai64.dll is in C:\Program Files (x86)\ZED SDK\bin

[ZED][INFO] Logging level INFO
[ZED][INFO] [Init] Depth mode: PERFORMANCE
[ZED][INFO] [Init] Camera successfully opened.
[ZED][INFO] [Init] Sensors FW version: 776
[ZED][INFO] [Init] Camera FW version: 1523
[ZED][INFO] [Init] Video mode: HD720@60
Object Detection: Loading Module…
CORRUPTED SDK INSTALLATION
[ZED][ERROR] sl_ai library loading failed details: “sl_ai64.dll”: The specified module could not be found.
[ZED][ERROR] [Object Detection] Missing sl_ai library
[ZED][ERROR] [ZED] [Object Detection] SL_AI_NOT_FOUND

Hi,
This can be related to the fact that you have either nvinfer.dll or cudnn64_8.dll somewhere else in your path (from a different version than the one requested and installed by the ZED SDK).
We are looking for a way to better handle this case.

Anyway we can chat about this offline?

sure, send an email to
support@stereolabs.com
with a link to this topic

I have the same error with SDK 4.0… Is it normal ?