Any idea why memory type indexing starts from 1? For instance, in Python api,
>>> sl.MEM(1)
<MEM.CPU: 1>
>>> sl.MEM(2)
<MEM.GPU: 2>
>>> sl.MEM(0)
Traceback (most recent call last):
File "<stdin>", line 1, in <module>
File "/home/ymtoo/anaconda3/lib/python3.8/enum.py", line 339, in __call__
return cls.__new__(cls, value)
File "/home/ymtoo/anaconda3/lib/python3.8/enum.py", line 663, in __new__
raise ve_exc
ValueError: 0 is not a valid MEM
Other enum types are fine.
>>> sl.ERROR_CODE(0)
SUCCESS
>>> sl.ERROR_CODE(1)
FAILURE
>>> sl.MAT_TYPE(0)
<MAT_TYPE.F32_C1: 0>
>>> sl.MAT_TYPE(1)
<MAT_TYPE.F32_C2: 1>
My setup:
- Ubuntu 20.04
- ZED SDK 3.6
- pyzed 3.6
Reference:
https://www.stereolabs.com/docs/api/group__Core__group.html#ga3fc8f9f9f84fbb0f728fc2cd399ade29